ada4411-3 don't work

AD技术支持您好:

我遇到一个比较棘手的问题,我使用的ADA4411-3芯片不工作;我使用的ADA4411-3器件手册上的参考原理图设计的,ADV7340芯片输出RGB视频信号给ADA4411-3进行滤波,但是ADA4411-3有输入信号无输出信号。

如下图为ADV7340的RGB信号输出,并联300欧姆电阻到gnd。

如下图为ADA4411-3的原理图,23管脚增益为4倍,1,24管脚幅度为600mV;15脚选择通道1,8,9管脚设置滤波通道00:36MHz;通道2无输入接下拉到gnd,通道1接RGB输入。

 

如图为ada4411-3输出并联75欧姆电阻到gnd,串联电容到VGA插座。

目前的问题是:在ADA4411-3芯片的RGB输出管脚上就没有发现信号输出;原因待查?

后来直接把ADA4411-3芯片的RGB输出75欧姆(R624,R625,R626)串联电阻不焊接将ADV7340的RGB输出信号接到输出电容(比如C1029~C1031)的前端,结果输出电容(比如C1029~C1031)的后端也没有信号,难道ADV7340的RGB输出信号是直流信号?直接被电容隔离了?

后来,电容也不接入电路了,直接将ADV7340的RGB输出信号接到输出电容(比如C1029~C1031)的后端,VGA有显示了。但是ADA4411-3电路也没用上,输出电容也没用上。

negon.meng@arrowasia.com

以上就是我的问题:1。Ada4411-3为什么没工作?2.输出电容是参照参考电路加的怎么也没用?

已发邮件附件给当地代理商,代理商回复无法解答,已转发技术中心;无响应,又发邮件附件给"china.support@analog.com"<china.support@analog.com>;,还是无响应,什么情况