ADICUP360: Sending a string through TX/RX Serial Communication

Hi,

I am using ADICUP360 for some time now and have been progressing with it, all thanks to the help that I get from this forum. I am intending to send some numbers / strings / chars from ADICUP 360 to another board via the serial TX/RX comm pins. However, I am unable to do so. I need a detailed explanation of how can this be made possible.


Currently, the switch configuration that I have set on ADICUP360 EVAL-BOARD is 0,1,0,1 (S1,S2,S3,S4). I am powering the board through the USER pin, the other end of which is connected to my laptop.

The code that I have written is:

UART_WriteString("fa"); //Send 'fa' on serial
timer_sleep (500);

I can read the string through PUTTY on my serial comm (with the corresponding switch config) but I am unable to read the data from TX/RX (PIN 1 and 2 on PWML). I would really appreciate if someone can help me out here. Also, I would like to know how can I use the other 3 TX/RX pins for sending data from the ADICUP360.

Thank You.