Hello
I want to use an external voltage of 3.3V for AD7794 to fully capture the signal.
Which voltage reference component you suggest me to choose?
And should I connect the REFIN- pin to the GND?
Thank you.
This was answered on another thread, so i copied it and pasted it below.
------------------------
Hi cevdet29,
The AD7794 suggests the use of ADR391 and ADR381 which are 2.5 V micropower low noise voltage…
The AD7794 suggests the use of ADR391 and ADR381 which are 2.5 V micropower low noise voltage reference.
For 3.3V, I suggest you use the ADR4533 which is ultra-low noise but has Is=950uA compared to the ADR391 with Is=120uA.
Yes you can connect the REFIN- pin to GND.
Btw the external reference can only accept 3.3V when AVdd is powered at 3.3V
Hope this helps.
ACatapang
-------------------------