/** * \file adrv9009/profiles/tx_bw100_ir122p88_rx_bw100_or122p88_orx_bw100_or122p88_dc122p88/talise_config.c * \brief Contains Talise configuration settings for the Talise API * * Copyright 2015-2017 Analog Devices Inc. * Released under the AD9378-AD9379 API license, for more information see the "LICENSE.txt" file in this zip file. * * The top level structure taliseDevice_t talDevice uses keyword * extern to allow the application layer main() to have visibility * to these settings. * * This file may not be fully complete for the end user application and * may need to updated for AGC, GPIO, and DAC full scale settings. * To create a full initialisation routine, the user should also refer to the * Iron Python initialisation routine generated by the GUI, and also the Talise User Guide. * */ #include "talise_types.h" #include "talise_config.h" #include "talise_error.h" #include "talise_agc.h" #ifdef ADI_ZYNQ_PLATFORM #include "zynq_platform.h" #endif int16_t txFirCoefs[40] = {6,-50,15,132,-64,-273,167,483,-329,-800,574,1286,-951,-2111,1433,3512,-1944,-6006,3234,17514,17514,3234,-6006,-1944,3512,1433,-2111,-951, 1286, 574,-800,-329,483,167,-273,-64,132,15,-50, 6}; int16_t rxFirCoefs[48] = {-7,-23,32, 51, -69,-113,143, 208,-257,-362, 436,590,-701,-925,1100,1424,-1746,-2348,2552,3709,-4378,-7342,9330,31458,31458,9330,-7342,-4378,3709,2552,-2348,-1746,1424,1100,-925,-701,590,436,-362,-257,208,143,-113,-69,51,32,-23,-7}; int16_t obsrxFirCoefs[48] = {-8,-20,31,45,-67,-100,137,186,-246,-324,415,530,-664,-832,1039,1281,-1651,-2125,2410,3339,-4172,-6546,9552,30554,30554,9552,-6546,-4172,3339,2410,-2125,-1651,1281,1039,-832,-664,530,415,-324,-246,186,137,-100,-67,45,31,-20,-8}; #ifdef ADI_ZYNQ_PLATFORM /** < Insert Customer Platform HAL State Container here>*/ /* * Platform Layer SPI settings - this structure is specific to ADI's platform layer code. * User should replace with their own structure or settings for their hardware */ zynqSpiSettings_t spiDev1 = { .chipSelectIndex = 1, .writeBitPolarity = 0, .longInstructionWord = 1, .CPHA = 0, .CPOL = 0, .mode = 0, .spiClkFreq_Hz = 25000000 }; /* * Platform Layer settings - this structure is specific to ADI's platform layer code. * User should replace with their own structure or settings for their hardware * The structure is held in taliseDevice_t below as a void pointer, allowing * the customer to pass any information for their specific hardware down to the * hardware layer code. */ zynqAdiDev_t talDevHalInfo = { .devIndex = 1, .spiSettings = &spiDev1, .spiErrCode = 0, .timerErrCode = 0, .gpioErrCode = 0, .logLevel = ADIHAL_LOG_ALL }; #endif /** * TalDevice a structure used by the Talise API to hold the platform hardware * structure information, as well as an internal Talise API state container * (devStateInfo) of runtime information used by the API. **/ taliseDevice_t talDevice = { #ifdef ADI_ZYNQ_PLATFORM /* Void pointer of users platform HAL settings to pass to HAL layer calls * Talise API does not use the devHalInfo member */ .devHalInfo = &talDevHalInfo, #else .devHalInfo = NULL, /* < Insert Customer Platform HAL State Container here>*/ #endif /* devStateInfo is maintained internal to the Talise API, just create the memory */ .devStateInfo = {0} }; taliseInit_t talInit = { /* SPI settings */ .spiSettings = { .MSBFirst = 1, /* 1 = MSBFirst, 0 = LSBFirst */ .enSpiStreaming = 0, /* Not implemented in ADIs platform layer. SW feature to improve SPI throughput */ .autoIncAddrUp = 1, /* Not implemented in ADIs platform layer. For SPI Streaming, set address increment direction. 1= next addr = addr+1, 0:addr=addr-1 */ .fourWireMode = 1, /* 1: Use 4-wire SPI, 0: 3-wire SPI (SDIO pin is bidirectional). NOTE: ADI's FPGA platform always uses 4-wire mode */ .cmosPadDrvStrength = TAL_CMOSPAD_DRV_2X /* Drive strength of CMOS pads when used as outputs (SDIO, SDO, GP_INTERRUPT, GPIO 1, GPIO 0) */ }, /* Rx settings */ .rx = { .rxProfile = { .rxFir = { .gain_dB = -6, /* filter gain */ .numFirCoefs = 48, /* number of coefficients in the FIR filter */ .coefs = &rxFirCoefs[0] }, .rxFirDecimation = 2, /* Rx FIR decimation (1,2,4) */ .rxDec5Decimation = 5, //4, /* Decimation of Dec5 or Dec4 filter (5,4) */ .rhb1Decimation = 1, /* RX Half band 1 decimation (1 or 2) */ .rxOutputRate_kHz = 184320, /* Rx IQ data rate in kHz */ .rfBandwidth_Hz = 150000000, /* The Rx RF passband bandwidth for the profile */ .rxBbf3dBCorner_kHz = 150000, /* Rx BBF 3dB corner in kHz */ .rxAdcProfile = {227,149,181,90,1280,699,1300,59,1302,32,855,27,48,46,32,194,0,0,0,0,49, 0,7,6,42,0,7,6,42,0,25,27,0,0,25,27, 0,0,165,44,31,905}, /* pointer to custom ADC profile */ .rxDdcMode = TAL_RXDDC_BYPASS, /* Rx DDC mode */ .rxNcoShifterCfg = { .bandAInputBandWidth_kHz = 0, .bandAInputCenterFreq_kHz = 0, .bandANco1Freq_kHz = 0, .bandANco2Freq_kHz = 0, .bandBInputBandWidth_kHz = 0, .bandBInputCenterFreq_kHz = 0, .bandBNco1Freq_kHz = 0, .bandBNco2Freq_kHz = 0 } }, .framerSel = TAL_FRAMER_A, /* Rx JESD204b framer configuration */ .rxGainCtrl = { .gainMode = TAL_MGC, /* taliserxGainMode_t gainMode */ .rx1GainIndex = 255, /* uint8_t rx1GainIndex */ .rx2GainIndex = 255, /* uint8_t rx2GainIndex */ .rx1MaxGainIndex = 255, /* uint8_t rx1MaxGainIndex */ .rx1MinGainIndex = 195, /* uint8_t rx1MinGainIndex */ .rx2MaxGainIndex = 255, /* uint8_t rx2MaxGainIndex */ .rx2MinGainIndex = 195 /* uint8_t rx2MinGainIndex */ }, .rxChannels = TAL_RX1RX2, /* The desired Rx Channels to enable during initialization */ }, /* Tx settings */ .tx = { .txProfile = { .dacDiv = 1, /* The divider used to generate the DAC clock */ .txFir = { .gain_dB = -6, /* filter gain */ .numFirCoefs = 40, /* number of coefficients in the FIR filter */ .coefs = &txFirCoefs[0] }, .txFirInterpolation = 2, /* The Tx digital FIR filter interpolation (1,2,4) */ .thb1Interpolation = 1, /* Tx Halfband1 filter interpolation (1,2) */ .thb2Interpolation = 1, /* Tx Halfband2 filter interpolation (1,2)*/ .thb3Interpolation = 1, /* Tx Halfband3 filter interpolation (1,2)*/ .txInt5Interpolation = 5, /* Tx Int5 filter interpolation (1,5) */ .txInputRate_kHz = 184320, /* Primary Signal BW */ .primarySigBandwidth_Hz = 100000000, /* The Rx RF passband bandwidth for the profile */ .rfBandwidth_Hz = 150000000, /* The Tx RF passband bandwidth for the profile */ .txDac3dBCorner_kHz = 187000, /* The DAC filter 3dB corner in kHz */ .txBbf3dBCorner_kHz = 75000, /* The BBF 3dB corner in kHz */ .loopBackAdcProfile = {265, 146, 181, 90, 1280, 366, 1257, 27, 1258, 17, 718, 39, 48, 46, 27, 161, 0, 0, 0, 0, 40, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905} }, .deframerSel = TAL_DEFRAMER_A, /* Talise JESD204b deframer config for the Tx data path */ .txChannels = TAL_TX1TX2, /* The desired Tx channels to enable during initialization */ .txAttenStepSize = TAL_TXATTEN_0P05_DB, /* Tx Attenuation step size */ .tx1Atten_mdB = 0, /* Initial Tx1 Attenuation */ .tx2Atten_mdB = 0, /* Initial Tx2 Attenuation */ .disTxDataIfPllUnlock = TAL_TXDIS_TX_RAMP_DOWN_TO_ZERO /* Options to disable the transmit data when the RFPLL unlocks. */ }, /* ObsRx settings */ .obsRx = { .orxProfile = { .rxFir = { .gain_dB = -6, /* filter gain */ .numFirCoefs = 48, /* number of coefficients in the FIR filter */ .coefs = &obsrxFirCoefs[0] }, .rxFirDecimation = 2, /* Rx FIR decimation (1,2,4) */ .rxDec5Decimation = 5, /* Decimation of Dec5 or Dec4 filter (5,4) */ .rhb1Decimation = 1, /* RX Half band 1 decimation (1 or 2) */ .orxOutputRate_kHz = 184320, /* Rx IQ data rate in kHz */ .rfBandwidth_Hz = 150000000, /* The Rx RF passband bandwidth for the profile */ .rxBbf3dBCorner_kHz = 225000, /* Rx BBF 3dB corner in kHz */ .orxLowPassAdcProfile = { 227,149, 181, 90, 1280, 699,1300,59, 1302,32, 855,27,48,46,32,194,0,0,0,0,49, 0, 7,6,42,0,7,6,42,0,25,27,0,0, 25,27,0, 0,165,44,31,905}, .orxBandPassAdcProfile = { 227,149, 181, 90, 1280, 699,1300,59, 1302,32, 855,27,48,46,32,194,0,0,0,0,49, 0, 7,6,42,0,7,6,42,0,25,27,0,0, 25,27,0, 0,165,44,31,905}, .orxDdcMode = TAL_ORXDDC_DISABLED, /* ORx DDC mode */ .orxMergeFilter = {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0} }, .orxGainCtrl = { .gainMode = TAL_MGC, .orx1GainIndex = 255, .orx2GainIndex = 255, .orx1MaxGainIndex = 255, .orx1MinGainIndex = 195, .orx2MaxGainIndex = 255, .orx2MinGainIndex = 195 }, .framerSel = TAL_FRAMER_B, /* ObsRx JESD204b framer configuration */ .obsRxChannelsEnable = TAL_ORX1ORX2, /* The desired ObsRx Channels to enable during initialization */ .obsRxLoSource = TAL_OBSLO_RF_PLL /* The ORx mixers can use the TX_PLL */ }, /* Digital Clock Settings */ .clocks = { .deviceClock_kHz = 184320, //184320, // 92160, /* CLKPLL and device reference clock frequency in kHz */ .clkPllVcoFreq_kHz = 7372800, /* CLKPLL VCO frequency in kHz */ .clkPllHsDiv = TAL_HSDIV_2, /* CLKPLL high speed clock divider */ .rfPllUseExternalLo = 0, /* 1= Use external LO for RF PLL, 0 = use internal LO generation for RF PLL */ .rfPllPhaseSyncMode = TAL_RFPLLMCS_INIT_AND_CONTTRACK /* RFPLL MCS (Phase sync) mode */ }, //Tx Profile IQrate and filter settings are not possible with current CLKPLL frequency /* JESD204B settings */ .jesd204Settings = { /* Framer A settings */ .framerA = { .bankId = 1, /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */ .deviceId = 0, /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */ .lane0Id = 0, /* JESD204B Configuration starting Lane ID. If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */ .M = 4, /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */ .K = 32, /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */ .F = 4, /* F (number of bytes per frame) */ .Np = 16, /* Np (converter sample resolution) */ .scramble = 1, /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */ .externalSysref = 1, /* 0=use internal SYSREF, 1= use external SYSREF */ .serializerLanesEnabled = 0x03, /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */ .serializerLaneCrossbar = 0xE4, /* serializerLaneCrossbar */ .lmfcOffset = 31, /* lmfcOffset - LMFC offset value for deterministic latency setting */ .newSysrefOnRelink = 0, /* newSysrefOnRelink */ .syncbInSelect = 0, /* syncbInSelect; */ .overSample = 0, /* 1=overSample, 0=bitRepeat */ .syncbInLvdsMode = 1, .syncbInLvdsPnInvert = 0, .enableManualLaneXbar = 0 /* 0=auto, 1=manual */ }, /* Framer B settings */ .framerB = { .bankId = 0, /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */ .deviceId = 0, /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */ .lane0Id = 0, /* JESD204B Configuration starting Lane ID. If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */ .M = 2, /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */ .K = 32, /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */ .F = 2, /* F (number of bytes per frame) */ .Np = 16, /* Np (converter sample resolution) */ .scramble = 1, /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */ .externalSysref = 1, /* 0=use internal SYSREF, 1= use external SYSREF */ .serializerLanesEnabled = 0x0C, /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */ .serializerLaneCrossbar = 0xE4, /* serializerLaneCrossbar */ .lmfcOffset = 31, /* lmfcOffset - LMFC offset value for deterministic latency setting */ .newSysrefOnRelink = 0, /* newSysrefOnRelink */ .syncbInSelect = 1, /* syncbInSelect; */ .overSample = 0, /* 1=overSample, 0=bitRepeat */ .syncbInLvdsMode = 1, .syncbInLvdsPnInvert = 0, .enableManualLaneXbar = 0 /* 0=auto, 1=manual */ }, /* Deframer A settings */ .deframerA = { .bankId = 0, /* bankId extension to Device ID (Valid 0..15) */ .deviceId = 0, /* deviceId link identification number. (Valid 0..255) */ .lane0Id = 0, /* lane0Id Lane0 ID. (Valid 0..31) */ .M = 4, /* M number of DACss (0, 2, or 4) - 2 DACs per transmit chain */ .K = 32, /* K #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */ .scramble = 1, /* scramble scrambling off if scramble= 0 */ .externalSysref = 1, /* externalSysref 0= use internal SYSREF, 1= external SYSREF */ .deserializerLanesEnabled = 0x0F, /* deserializerLanesEnabled bit per lane, [0] = Lane0 enabled */ .deserializerLaneCrossbar = 0xE4, /* deserializerLaneCrossbar */ .lmfcOffset = 17, /* lmfcOffset LMFC offset value to adjust deterministic latency */ .newSysrefOnRelink = 0, /* newSysrefOnRelink */ .syncbOutSelect = 0, /* SYNCBOUT0/1 select */ .Np = 16, /* Np (converter sample resolution) */ .syncbOutLvdsMode = 1, .syncbOutLvdsPnInvert = 0, .syncbOutCmosSlewRate = 0, .syncbOutCmosDriveLevel = 0, .enableManualLaneXbar = 0 /* 0=auto, 1=manual */ }, /* Deframer B settings */ .deframerB = { .bankId = 0, /* bankId extension to Device ID (Valid 0..15) */ .deviceId = 0, /* deviceId link identification number. (Valid 0..255) */ .lane0Id = 0, /* lane0Id Lane0 ID. (Valid 0..31) */ .M = 0, /* M number of DACss (0, 2, or 4) - 2 DACs per transmit chain */ .K = 32, /* K #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */ .scramble = 1, /* scramble scrambling off if scramble= 0 */ .externalSysref = 1, /* externalSysref 0= use internal SYSREF, 1= external SYSREF */ .deserializerLanesEnabled = 0x00, /* deserializerLanesEnabled bit per lane, [0] = Lane0 enabled */ .deserializerLaneCrossbar = 0xE4, /* deserializerLaneCrossbar */ .lmfcOffset = 0, /* lmfcOffset LMFC offset value to adjust deterministic latency */ .newSysrefOnRelink = 0, /* newSysrefOnRelink */ .syncbOutSelect = 1, /* SYNCBOUT0/1 select */ .Np = 16, /* Np (converter sample resolution) */ .syncbOutLvdsMode = 1, .syncbOutLvdsPnInvert = 0, .syncbOutCmosSlewRate = 0, .syncbOutCmosDriveLevel = 0, .enableManualLaneXbar = 0 /* 0=auto, 1=manual */ }, .serAmplitude = 15, /* Serializer amplitude setting. Default = 15. Range is 0..15 */ .serPreEmphasis = 1, /* Serializer pre-emphasis setting. Default = 1 Range is 0..4 */ .serInvertLanePolarity = 0, /* Serializer Lane PN inversion select. Default = 0. Where, bit[0] = 1 will invert lane [0], bit[1] = 1 will invert lane 1, etc. */ .desInvertLanePolarity = 0, /* Deserializer Lane PN inversion select. bit[0] = 1 Invert PN of Lane 0, bit[1] = Invert PN of Lane 1, etc */ .desEqSetting = 1, /* Deserializer Equalizer setting. Applied to all deserializer lanes. Range is 0..4 */ .sysrefLvdsMode = 1, /* Use LVDS inputs on Talise for SYSREF */ .sysrefLvdsPnInvert = 0 /*0= Do not PN invert SYSREF */ } }; //Only needs to be called if user wants to setup AGC parameters static taliseAgcCfg_t rxAgcCtrl = { 4, 255, 195, 255, 195, 30720, /* AGC gain update time in us (125us-250us - based on IQ data rate - set for 125us @ 184.32 Mhz) */ 10, 10, 16, 0, 1, 0, 0, 0, 1, 31, 246, 4, 1, /*!<1- bit field to enable the multiple time constants in AGC loop for fast attack and fast recovery to max gain. */ /* agcPower */ { 1, /*!<1-bit field, enables the Rx power measurement block. */ 1, /*!<1-bit field, allows using Rx PFIR for power measurement. */ 0, /*!<1-bit field, allows to use the output of the second digital offset block in the Rx datapath for power measurement. */ 9, /*!