diff --git a/drivers/iio/adc/ad9371.c b/drivers/iio/adc/ad9371.c index 68fef24..930ebbf 100644 --- a/drivers/iio/adc/ad9371.c +++ b/drivers/iio/adc/ad9371.c @@ -570,7 +570,8 @@ static int ad9371_init_cal(struct ad9371_rf_phy *phy, uint32_t initCalMask) uint8_t status = 0; mykonosInitCalStatus_t initCalStatus; mykonosErr_t mykError; - + + printk("!!!!My Debugger init_call_mask %X\n", initCalMask); /*****************************************************/ /*** Mykonos ARM Initialization Calibrations ***/ /*****************************************************/ @@ -661,6 +662,8 @@ static int ad9371_setup(struct ad9371_rf_phy *phy) TX_ATTENUATION_DELAY | RX_GAIN_DELAY | FLASH_CAL | PATH_DELAY | LOOPBACK_RX_LO_DELAY | LOOPBACK_RX_RX_QEC_INIT | RX_LO_DELAY; + + printk("My Debugger init_call_mask %X\n", initCalMask); if (has_rx_and_en(phy)) phy->tracking_cal_mask |= TRACK_RX1_QEC | TRACK_RX2_QEC; @@ -891,8 +894,9 @@ static int ad9371_setup(struct ad9371_rf_phy *phy) /*****************************************************/ /*** Mykonos ARM Initialization Calibrations ***/ /*****************************************************/ - + printk("My Debugger init_call_mask %X\n", initCalMask); ret = ad9371_init_cal(phy, initCalMask); + printk("My Debugger init_call_mask %X\n", initCalMask); if (ret != MYKONOS_ERR_OK) { dev_err(&phy->spi->dev, "%s (%d)", getMykonosErrorMessage(ret), ret); @@ -1203,7 +1207,7 @@ static ssize_t ad9371_phy_store(struct device *dev, phy->cal_mask &= ~val; } else if (enable) { ad9371_set_radio_state(phy, RADIO_FORCE_OFF); - + ret = ad9371_init_cal(phy, phy->cal_mask); if (ret != MYKONOS_ERR_OK) { dev_err(&phy->spi->dev, "%s (%d)", @@ -3013,7 +3017,7 @@ static struct ad9371_phy_platform_data AD9371_OF_PROP("adi,default-initial-calibrations-mask", &phy->init_cal_mask, TX_BB_FILTER | ADC_TUNER | TIA_3DB_CORNER | DC_OFFSET | TX_ATTENUATION_DELAY | RX_GAIN_DELAY | FLASH_CAL | - PATH_DELAY | TX_LO_LEAKAGE_INTERNAL | TX_QEC_INIT | + PATH_DELAY | TX_LO_LEAKAGE_INTERNAL | /*TX_QEC_INIT |*/ LOOPBACK_RX_LO_DELAY | LOOPBACK_RX_RX_QEC_INIT | RX_LO_DELAY | RX_QEC_INIT | (IS_AD9375(phy) ? DPD_INIT | CLGC_INIT | VSWR_INIT: 0)); @@ -4414,8 +4418,9 @@ static int ad9371_jesd204_setup_stage1(struct jesd204_dev *jdev, TX_ATTENUATION_DELAY | RX_GAIN_DELAY | FLASH_CAL | PATH_DELAY | LOOPBACK_RX_LO_DELAY | LOOPBACK_RX_RX_QEC_INIT | RX_LO_DELAY; - + printk("My Debugger init_call_mask %X\n", phy->init_cal_mask); ret = ad9371_init_cal(phy, phy->init_cal_mask); + printk("My Debugger init_call_mask %X\n", phy->init_cal_mask); if (ret != MYKONOS_ERR_OK) { dev_err(&phy->spi->dev, "%s (%d)", getMykonosErrorMessage(ret), ret);