Post Go back to editing

Analog Device BLIP2 Board Questions.

Hello,

We are working on a proposal which involves mating a camera sensor to a custom board. We were hoping to use the BLIP2 platform to prototype this.

Could you get us in touch with the developer who created the kit and answer the below queries:

Questions:

1. Our requirement is to interface 12 to 18Megapixel cameras. The highest VGA camera that the BLIP2 can handle is a 2MP(640x480) camera from Aptina or Omnivision.

Can a higher resolution camera be interfaced with the BLIP2. If yes, what changes does it involve. 

2. The cameras that come with the kit have an ePPI interface. Does the kit support MiPi? 

eg: Jetson TK1 camera board | NVIDIA camera | TK1 camera module 

Can ADI support us in this endeavor.

3. How does the software licensing work in this case? Would we have full access to the kernel and source code?

4. The current kit example streams video data and analyzes it. We plan to capture images @1Hz and store them into the SD card. Is this possible.

5. Can the captured data be copied from the SD card into a host PC... or describing it another way, does the USB support Mass Storage Class(MSC).

We are on a tight schedule to research and deliver. I can hop on a call with the team here if needed. 

Thanks,

-Gerard

  • Hi Gerard,

    I forwarded your questions to the apps. engineer for the BLIP platform and will get back to you shortly.

    Best Regards,

    Bill.

  •  

    Analog Device BLIP2 Board Questions.

    created by Gseq in Boston Engineering Collaboration Group - View the full discussion

    Hello,

    We are working on a proposal which involves mating a camera sensor to a custom board. We were hoping to use the BLIP2 platform to prototype this.

    Could you get us in touch with the developer who created the kit and answer the below queries

     

    Questions:

    1. Our requirement is to interface 12 to 18Megapixel cameras. The highest VGA camera that the BLIP2 can handle is a 2MP(640x480) camera from Aptina or Omnivision.

    Can a higher resolution camera be interfaced with the BLIP2. If yes, what changes does it involve. 

    One way is to re-spin BLIP2 to replace the VGA camera by a higher resolution camera, assuming the latter supports parallel output (such as DVP). If the camera only supports differential output (e.g. MIPI), a bridge device is needed to convert the differential to parallel. Lattice FPGA is one choice for the bridge. Alternatively, if the camera supports USB output, it can be connected to the USB port of BLIP2. In this case, BLIP2 must be configured as the host.

    2. The cameras that come with the kit have an ePPI interface. Does the kit support MiPi? 

    eg: Jetson TK1 camera board | NVIDIA camera | TK1 camera module 

    Can ADI support us in this endeavor.

    No, BLIP2 does not support MIPI. MIPI is on the roadmap but is currently not supported. A bridge device (like a Lattice FGPA) would be required to convert MIPI to ePPI.

    3. How does the software licensing work in this case? Would we have full access to the kernel and source code?

    Binary code is offered free of charge (available for download from www.analog.com/blip). Source code would be under separate contract. Please contact ADI sales team.

    4. The current kit example streams video data and analyzes it. We plan to capture images @1Hz and store them into the SD card. Is this possible.

    BLIP2 has a connector for SD card.

    5. Can the captured data be copied from the SD card into a host PC... or describing it another way, does the USB support Mass Storage Class(MSC).

    The USB currently only supports Bulk transfer. It does not support MSC. It should be possible to modify the BLIP firmware to copy SD card to PC via the USB Bulk link.

    I can hop on a call with the team here if needed.

     

     

     

    Reply to this message by replying to this email, or go to the message on EngineerZone

    Start a new discussion in Boston Engineering Collaboration Group by email or at EngineerZone

    Following Boston Engineering Collaboration Group in these streams: Email Watches

    This email was sent by EngineerZone because you are a registered user. You may unsubscribe instantly from EngineerZone, or adjust email frequency in your email preferences

  • Thank you. Do you have time tomorrow to hop on a call?

  • Hi Gerad,

    The product apps. engineer for the BLIP is not available for direct support at this time. He suggested that you submit your question to the BLIP support team, via the Analog Devices Engineer Zone @ Embedded Vision Sensing 

    Please be aware that this is a public facing site. 

    Best Regards,

    Bill.