Hello! This is a follow up to my previous question here: https://ez.analog.com/boston-engineering/f/q-a/117280/cn-0359-accuracy-question
It was mentioned by charlyelkhoury that the CN-0359 uses an auto-ranging feature to determine what the sensing range for conductivity will be. In order to determine the accuracy in mS/cm I will need to know what the auto-ranging function is setting the range to. Could someone please tell me where in the CN-0359 firmware this feature is located?
Additionally it is stated in the user manual that the accuracy is 0.6% FS. Is this +/- 0.6% or +/-0.3% which would add up to a total of 0.6%?
Thank you!