Analog Devices Completes Acquisition of Hittite Microwave Corporation

  • Analog Devices recently announced the completion of its acquisition of Hittite Microwave Corporation. With the addition of these new products now known as Hittite Microwave products from Analog Devices, ADI strengthens its innovation engine across RF, microwave, and millimeter wave applications and creates even greater value for customers by addressing the entire frequency spectrum with over 2,000 products from antenna to bits and back. Complemented by the world's leading data converters, Analog Devices is the only single source supplier to cover the entire signal chain. Learn more and access FAQs at www.analog.com/hittite.
  New Production Released Products 

Converters

  • ADE7878A Polyphase, Multifunction, Energy Metering IC with per Phase Active and Reactive Powers
  • ADE7868A  Polyphase, Multifunction, Energy Metering IC with Tamper Detection and Low Power Mode
  • ADE7858A  Polyphase, Multifunction, Energy Metering IC with per Phase Active and Reactive Powers
  • ADE7854A  Polyphase, Multifunction Energy Metering IC
  Amplifiers 
  • ADA4805-1  0.2 µV/°C Offset Drift, 105 MHz Low Power, Low Noise, Rail-to-Rail Amplifier

RF/IF ICs

·        ADL6010  Fast Responding, 45 dB Range, 0.5 GHz to 43.5 GHz Envelope Detector

Power Management

·        ADM1278 Hot Swap Controller and Digital Power and Energy Monitor with PMBus Interface

Interface and Isolation

  • ADuM3150  3.75 kV, 6-Channel, SPIsolatorTm Digital Isolator for SPI with Delay Clock
  • ADuM3151  3.75 kV, 7-Channel Isolator for SPI Interfaces (5-Channel/2-Channel Directionality)
  • ADuM3152  3.75 kV, 7-Channel Isolator for SPI Interfaces (4-Channel/3-Channel Directionality)
  • ADuM3153  3.75 kV, 7-Channel Isolator for SPI Interfaces (3-Channel/4-Channel Directionality)
  • ADuM3154  3.75 kV, 7-Channel Digital Isolator for SPI Interfaces
  Motor Control Evaluation System 

New Parts—Sampling Stage

  • ADA4701-1  High Voltage (100 V) Precision Amplifier
  New Sales Tools and Collateral    Circuits from the LabRegistered Reference Design program    Videos 

Webcasts

  Technical Articles    Events 
  • A3E Audio Conference, ADI’s DSP audio group will be at this year’s show in Boston, September 23 to 24, 2014, Hynes Convention Center, Boston, MA, U.S.A.
  • Learn more about ADI’s expanded RF and microwave portfolio at ADI’s Booth #232, European Microwave Week, October 7 to 9, Fiera di Roma, Rome, Italy
  Blogs 

Our relationship with you is very important. To manage your newsletter subscriptions, visit our subscription center.
To unsubscribe from surveys by Analog Devices, please click here.
To no longer receive any further email communications from Analog, please click here.View our privacy policy.

Copyright 2014 Analog Devices, Inc. All Rights Reserved. Trademarks and registered trademarks are the property of their respective companies.
Analog Devices, Inc.
Corporate Headquarters
3 Technology Way
Norwood, MA 02062
U.S.A.

Anonymous