Analog Devices to Acquire Hittite Microwave Corporation

  • Analog Devices, Inc. (NASDAQ: ADI), a global leader in high performance semiconductors for signal processing applications, and Hittite Microwave Corporation (NASDAQ:HITT), an innovative designer and manufacturer of high performance integrated circuits, modules, subsystems, and instrumentation for RF, microwave, and millimeter wave applications, announced on June 9, 2014 that the two companies have entered into a definitive agreement whereby ADI will acquire Hittite. For more details, please view the press release here.
  New Production Released Products 

Amplifiers

  • ADA4870  High Speed, High Voltage, 1 A Output Drive Amplifier
  • ADA4610-4  Low Noise, Precision, Rail-to-Rail Output, JFET Quad Operational Amplifier
  • AD8285 Radar Receive Path AFE: 4-Channel LNA/PGA/AAF with ADC
  RF/IF ICs 
  • ADF4155  Integer-N/Fractional-N PLL Synthesizer

Power Management

  Interface and Isolation 
  • AD7403  16-Bit, Isolated Σ-Δ Modulator
  • SPIsolatorTM  Newest family of digital isolators for SPI interfaces
  Processors and DSP    New Parts—Sampling Stage 
  • ADuM3150  3.75 kV, 6-Channel Isolator for SPI Interfaces 
  • ADuM3151  3.75 kV, 7-Channel Isolator for SPI Interfaces (5/2 channel directionality)
  • ADuM3152  3.75 kV, 7-Channel Isolator for SPI Interfaces (4/3 channel directionality)
  • ADuM3153  3.75 kV, 7-Channel Isolator for SPI Interfaces (3/4 channel directionality)
  • ADuM3154  3.75 kV, 7-Channel Digital Isolator for SPI Interfaces
  • AD9625 12-Bit, 2.5 GSPS, 1.3 V/2.5 V ADC
  • ADA4961  Low Distortion, 2.5 GHz, Differential DGA 
  • ADRF6612  700 MHz to 3000 MHz Dual Passive Receive Mixer with Integrated PLL and VCO
  • ADA4084-1  30 V Low Power, Low Noise RRIO Single Operational Amplifier
  • ADA4805-2  5.9 nV/√Hz, 480 µA, 100 MHz Rail-to-Rail Output Amplifier for Driving 16-bit SAR ADC
  New Sales Tools and Collateral 
  • View the latest release of the Industrial Control presentations:
    • Products—Industrial Control: comprehensive product presentation with the latest releases for industrial control (sections updated include precision ADCs and DACs, amplifiers, integrated amplifiers, power management, iSensors, and embedded processing—DSP)
    • Applications—Industrial Control: detailed signal chains, recommended products, Circuits from the Lab, and support resources (next update due 4Q14)
  • Additional resources for the ADSP-BF70x BlackfinRegistered processor family, a high performance DSP series that delivers a class-leading 800 MMACS of processing power at less than 100 mW—double the performance or half the power of competing devices.
  • SVPP for Jul-Aug-Sept 2014 Broad Market Select products is now in a content pack on SFDC and Distributor Portal (keyword: “SVPP” or “select products”). In this content pack, you will find the SVPP (in PowerPoint and PDF formats) and FAQ for training, as well as a customer oriented set of product overviews.
  Events 
  • Analog Devices Sponsors X-fest 2014  Register now for this global series of seminars offering practical, how-to training for FPGA, SoC, DSP, and embedded systems designers. From September 2014 through January 2015, X-fest training events will be hosted in nearly 40 locations throughout Asia, Europe, North America, and Japan.

Our relationship with you is very important. To manage your newsletter subscriptions, visit our subscription center.
To unsubscribe from surveys by Analog Devices, please click here.
To no longer receive any further email communications from Analog, please click here.View our privacy policy.

Copyright 2014 Analog Devices, Inc. All Rights Reserved. Trademarks and registered trademarks are the property of their respective companies.
Analog Devices, Inc.
Corporate Headquarters
3 Technology Way
Norwood, MA 02062
U.S.A.

Anonymous