DavidHTO

The Day I Joined the Space Race

Blog Post created by DavidHTO Employee on May 3, 2018

I’m back again to talk about my hobby of ham radio. Last time I wrote about the experimental antenna I recently built on my property for operating on the low (1.8 – 2.0 MHz) Amateur Radio bands. Today I’m going to go back to my early days in the hobby when I first got to know OSCAR. No, not the Grouch or Felix’s roommate, this was the acronym for the Orbiting Satellite Carrying Amateur Radio. 

 

Hams have always been at the forefront of communication technology, starting with the first wireless stations which sent and received Morse code. Hams would later experiment with some of the first AM, FM, and even television stations, so it’s no surprise that they were early in communication utilizing space. In fact, the Space Race was only four years old when OSCAR 1 was launched on December 12, 1961. OSCAR 1 was a very humble beginning to ham radio in space, as it was literally used as ballast to balance the payload of the rocket, although it holds the distinction of being the first satellite to be ejected as a secondary payload and enter a separate orbit. According to the OSCAR Wikipedia page, “…the satellite carried no on-board propulsion and the orbit decayed quickly. Despite being in orbit for only 22 days, OSCAR 1 was an immediate success with over 570 amateur radio operators in 28 countries forwarding observations to Project OSCAR.”

 

In 1974 after a series of successful launches of increasingly sophisticated satellites, Oscar 7 was launched, and that was followed fours later by the launch of Oscar 8. Both satellites were in low earth orbit (about 115 – 120 miles up) which meant they would only be in range at certain times and for a short period of time, but could both send and receive Morse code signals, permitting actual conversations. Both satellites acted as “repeaters,” receiving signals (the uplink) on the 2-meter band (144 – 148 MHz) and transmitting on the ten-meter band (28.000 – 29.000.)  As a youngster who grew up thrilled by the exploits of Shepard, Grissom, and Glenn it was exciting to think that in some small way I could experience the Space Program first-hand. Using a polar azimuth projection of the earth and a plastic overlay of Oscar 7 orbits (which had been included in an issue of QST, a ham radio magazine) it was easy to determine when the satellite would pass within range.

 

Azimuthal projection

From an edition of QST magazine.  Plastic overlays (with either Oscar 7 or 8 orbital paths) sat over this map

 

I set my transceiver (the rig was a Tempo One) to the down-link frequency on 10 meters and, when the timing was right, I could actually hear a number of CQs and QSOs coming from space. That was pretty cool. But I knew that the real fun would begin when I transmitted through the satellite, and so in the spring of 1977 I bought a used Hallicrafters VHF1 “Seneca” 2 meter transmitter, then constructed a 2-meter ground plane out of coat hangers, which I hung outside the shack window. Nothing fancy, as I had recently purchased a used TH3 beam for mounting on my parent's roof (these were GREAT parents) and knew eventually I would stack some sort of antenna for 144 - 148 MHz up there. Once I had the 2-meter transmitter working, I checked my QST Magazine for the satellite's latest schedule and, with my high-tech plastic overlay, saw that Oscar 7 would pass right over New York on the afternoon of June 6th, 1977.

 

OSCAR 7

A rendering of OSCAR 7 

 

I started hearing CW signals from other stations a few minutes after 1:00 pm (EDT) on 10 meters and began sending CQ (the internationally recognized abbreviation for “calling any station”) on 2 meters (remember that OSCAR was a 2 meter receive/10 meter transmit repeater). That’s when I heard… nothing. Huh. Well, since I didn't have a directional antenna I kind of figured the satellite, which was orbiting about 115 miles above, would have to be a lot closer to pick me up. So I tried again and - BINGO! - there it was, coming back to me on 10 meters, my own signal! Now here's the really cool part: as I'm transmitting and the satellite is racing towards me at 17,000 miles an hour, I could hear the tone of the signal getting higher in pitch - the Doppler shift of my signal coming back from space. It got stronger too, as Oscar 7 passed almost directly overhead, then almost immediately the tones began to shift lower as the bird raced away and the opposite Doppler shift took effect. Well, I just thought that was the coolest thing to be able to actually hear that happening. As of this blog, the experience is as vivid as any ham radio memory I have. 

 

Repeated attempts at connecting with another station were unsuccessful, not surprising given the transmit antenna was non-directional and, geez, made of coat hangers. Two weeks later I installed the TH3 beam (for 10, 15, and 20 meters) and a Cushcraft circularly polarized 2-meter antenna, stacked on top of the HF beam. Here’s how it looked shortly after installation. (My mom says she still gets heart palpitations thinking about me climbing on the roof.)

 

Kruh residence in New York, topped with two beamsThe roof of my parent's home in Merrick.

That's me, my TH3 HF beam and Cushcraft 2 meter antenna.

 

With both transmit and receive directional antennas in place, I was ready to go for a contact during OSCAR’s next pass.  On July 24, 1977 (Oscar 7's 12,294th orbit) I made my first space-based QSO, with a ham in Florida (WA4JID). I subsequently would connect with dozens of hams up and down the Eastern Seaboard and western Europe through Oscar 7 and then, in the summer of 1978, dozens more through Oscar 8. Yet I don't recall any of those QSOs as vividly as I do when I first heard the dits and dahs of my Doppler-shifted CW signal coming back at me from space.

Outcomes