Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Automated Test Equipment (ATE)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Automated Test Equipment (ATE)
Automated Test Equipment (ATE)
Documents MAX9979: FAQ PMU Functionality
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • -Documents
    • +AD5522 FAQs
    • +AD5560 FAQs
    • +MAX9959: FAQ
    • +MAX9972: FAQ
    • -MAX9979: FAQ
      • MAX9979: FAQ Driver Operation Range
      • MAX9979: FAQ Impedance Termination at DUT_pin
      • MAX9979: FAQ PMU Functionality
      • MAX9979: FAQ Power Dissipation
      • MAX9979: FAQ Voltage Clamps of Driver

MAX9979: FAQ PMU Functionality

If the VHH, +13V output is not required, then is it required to provide the +17V VHHP to  MAX9979 IC? Can only PMU functionality be utilized without applying +17V to the VHHP pin?

Even if super voltage (VHH) features of MAX9979 are not used, device operation still requires the user to apply VHHP. When VHHP is not applied, PMU functionality is not enabled.  There is an internal logic (watchdog) circuitry connecting PMU and VHHP circuitry.

  • Share
  • History
  • More