Hi experts
What's the difference between AD5522JSVUZ-RL and AD5522JSVUZ,temperature range shows different.
Which range is correct ?

| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 18 hours |
thomas.abiog BruceP jcabuhayan alank MacManato yyang2 mench |
Awaiting Company Response |
AD5522
Production
The AD5522 is a high performance, highly integrated parametric measurement unit consisting of four independent channels. Each per-pin parametric measurement...
Datasheet
AD5522 on Analog.com
Hi experts
What's the difference between AD5522JSVUZ-RL and AD5522JSVUZ,temperature range shows different.
Which range is correct ?

ianguieb - Moved from Specialty Amplifiers to Automated Test Equipment (ATE). Post date updated from Tuesday, February 17, 2026 6:50 AM UTC to Wednesday, February 18, 2026 1:36 AM UTC to reflect the move.
ianguieb - Moved from Specialty Amplifiers to Automated Test Equipment (ATE). Post date updated from Wednesday, February 18, 2026 1:36 AM UTC to Wednesday, February 18, 2026 1:36 AM UTC to reflect the move.
Hi TrashBoat ,
I moved this query to this community. Someone here should be able to help you.
Regards,
Ian
Hi ianguieb ,
Thank you for moving this to the ATE forum.
Hi TrashBoat ,
Thank you for reaching out.
The AD5522JSVUZ and AD5522JSVUZ-RL are the same device. The only difference is the packaging type:
Any variation shown in the ordering guide is packaging-related only and does not affect the device specifications.
The junction temperature (Tj) range for both models is 25°C to 90°C.
Best regards,
Judith
Hi Judith
Thank you for your response !
I will take it into consideration.
Best,