Post Go back to editing

ad5522 with AVDD+12V AVSS-12V FOH & MEASOUT output does‘t match in FIMV mode

Category: Hardware
Product Number: AD5522

Hi:

    Ad5522 avdd=12V, avss=-12V, vref=5V, configed as FIMV mode, force current = -100uA, current range = 200uA,  FOH = -500mV,  but MEASOUT = 1912mV,  according to datasheet, MEASOUT shoule be 2150mV. However, when avdd = 15V, avss=-15V, MEASOUT was correct (around 2150mV). Should I adjust software config or something else? 

Edit Notes

Add current range description.
[edited by: lastsword at 7:05 AM (GMT -5) on 9 Dec 2025]

Thread Notes

Parents
  • Hi,  

    Thanks for your question.

    To help us understand more about your inquiries, I have these following questions:

    1. What is your load in performing this test?

    2. Is the -500mV a measured value at the FOH?

    3. What are your gain settings?

    4. Are you using the customer evaluation board and software?

    5. Did you adjust your Offset DAC setting?

    Best regards,
    Mac

  • 1.ESD Protection Diode of GPIO.

    2.Yes, measured by a voltage meter.

    3.Measure current gain = 10,Measure OUT Gain = 0.2.

    5.No. 0xA492.

    4.We bought a EVA board recently, and the same behavior was observed. The linearity of MV is perfect, but has a Significant offset(Several hundred mV). ​The issue is currently resolved through software calibration. Is there better solution?

    Thanks for your time!

Reply
  • 1.ESD Protection Diode of GPIO.

    2.Yes, measured by a voltage meter.

    3.Measure current gain = 10,Measure OUT Gain = 0.2.

    5.No. 0xA492.

    4.We bought a EVA board recently, and the same behavior was observed. The linearity of MV is perfect, but has a Significant offset(Several hundred mV). ​The issue is currently resolved through software calibration. Is there better solution?

    Thanks for your time!

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.