Post Go back to editing

ad5522 with AVDD+12V AVSS-12V FOH & MEASOUT output does‘t match in FIMV mode

Category: Hardware
Product Number: AD5522

Hi:

    Ad5522 avdd=12V, avss=-12V, vref=5V, configed as FIMV mode, force current = -100uA, current range = 200uA,  FOH = -500mV,  but MEASOUT = 1912mV,  according to datasheet, MEASOUT shoule be 2150mV. However, when avdd = 15V, avss=-15V, MEASOUT was correct (around 2150mV). Should I adjust software config or something else? 

Edit Notes

Add current range description.
[edited by: lastsword at 7:05 AM (GMT -5) on 9 Dec 2025]

Thread Notes