Hi, I am interesting system level calibration of AD5522. (I mean self calibration or calibration without any additional instruments.)
I read the below thread but still don't clearly understand how we handle system level calibration after power-on.
MI calibration method of AD5522
So, At the AD5522 datasheet page 39 i assume that we not need any additional DUT or board or instrument for system level calibration.
FV mode for instance datasheet explain 2 point calibration.
Connect SYS_FORCE to FOHx and SYS_SENSE to MEASVHx. and load FIN dac 0x0000 and 0xFFFF then activate internal 10K resistor by closing SW7 switch. And using system PMU measure errors.
First of all SYS_FORCE and FOHx is can connected each other. if I can turn on 60 OHM switch. (Same as SYS_SENSE to MEASHVx.)

Secondly what is that mean "Using the system PMU, measure the error between the voltage at FOHx/MEASVHx and the desired value". Normally we should tight up FOHx and MEASVHx pins together.
I can't clearly understand the procedure. Can someone explain me how we can execute system level calibration?
Thanks
Oki