Post Go back to editing

Formula to measure voltage

Category: Datasheet/Specs
Product Number: AD5522

Hi,

I have a problem with the MV voltage formula with the AD5522.

Currently, I use the formula below for the current and it works fine. But the formula for the voltage gives me negative numbers. Am I using the right formula?

For example (Vref = 5V):

Vdut = 0V => Out = -2.24 (Vmin = 11.249)

Vdut = 4V => Out = -1.449 (Vmin = 11.249)

It is written in point 2 that OFFSET DAC, does not change the value of the output voltage. However, this is part of the formula ?

Thanks

Parents Reply Children
No Data