Hello.
I have a few questions about the AD5560. Please tell me.
Q1:Does the AD5560 offer lamp up/down control?
Q2:The datasheet includes the followin statement.
”The fastest ramp rate is 0.775 V/µs (for a 5 V reference and an 833 kHz clock using a 2032 LSB step size and divider = 1).”
How was SR calculated and determined at this time?
This is because when I calculated it, the calculated value was 0.645V/us, which did not match the data sheet value.
I calculated as below.
・1step = 16LSB (6.1mV), so it takes about 820steps to reach 5V.
・The update rate is 833 kHz, which is about 1.2 us for 1 step time.
・It takes about 7.74us to reach 5V, so the calculation is now 0.645V/us.
Best regards.