Post Go back to editing

We are not using the mid current range output. What do I tie its power supplies to ?

Category: Datasheet/Specs
Product Number: AD5560

We do not plan to use the mid current range output (the 500mA port).    What should I connect HCAVDD2 and HCAVSS2 to ?    GROUND or leave them floating ?   or should I make something like two 10K ohm voltage dividers to 50% of AVDD and AVSS ?   that is supplying a bias voltage, but little current.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.