We are evaluating MAX9979 using equipment.
We apologize for the inconvenience, but please check the following:
thank you.
Is the range value the limit for current measurement and current application?
For example, for the 2mA range, for the range -2mA to +2mA,
Is it possible to apply (FI) and measure (M) up to about 2.1mA on the positive side and -2.1mA on the negative side?
When I checked the operation, I was able to supply more than 2mA on the positive side, but I could only draw -2.0mA on the negative side.
(The intention of the question is for the 2mA range, so up to about -2.1mA.
It means that you want to respond)