Post Go back to editing

AD5560 calibration

Category: Hardware
Product Number: AD5560
Software Version: NONE

Hello,

In the AD5560 datasheet, I looked for information related to calibration. However, for the current measurement results, can we only simply adjust by addition or subtraction? For example, when it's 33mA, the error is 75μA. Then, in the data processing of the upper computer, I correct by 75μA. But when it's 10mA or 100mA, this error is no longer 75μA. Is there a solution for this? Another question: Can the AD5560 only measure the voltage it provides itself? If I don't set any voltage output for the AD5560 and directly connect the output to a 2V power source, the MEASOUT won't measure any values. Moreover, the 2V seems to be absorbed by the AD5560 since the voltmeter reads 0V at the output at that time.

Thank you.

Parents Reply Children
No Data