Hola
In the AD5560 datasheet, "The clamp circuitry compares the voltage across the sense resistor (multiplied by an in-amp gain of 10 or 20) to compare to the programmed clamp limit and activates the clamp circuit if either the high level or low level is exceeded, thus ensuring that the DUT current can never exceed the programmed clamp limit + 10% of full-scale current."
For example, when Clamp alarm status would be flagged when clamp current set to 1mA at I range in 25mA? 1mA? or 3.5mA?