MAX32000
Last Time Buy
The MAX32000 is a fully integrated, quad-channel, high-performance pin-electronics driver with built-in level-setting DACs, ideal for memory and SOC ATE...
Datasheet
MAX32000 on Analog.com
Hi All, out to.
What is the function of "Low Leak" and "High Imepedance Receive" mode in pin electronics MAX32000 ?
Regards, JJ
Hi JJ,
In MAX32000 "Low Leak" mode, you have the lowest leakage (nA range) at the DUT_ pins and there is essentially no functionality from MAX32000. In "High Impedance Receive", the leakage is higher (uA range) but the comparator, and the OVHV and OVLV (over voltage) are functional.
Hope this answers your question.
Regards,
Hooman
Hi Hooman,
Many thanks for the explanation.
Really very helpful, JJ
Hi Hooman,
Many thanks for the explanation.
Really very helpful, JJ