KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX32000
Last Time Buy
The MAX32000 is a fully integrated, quad-channel, high-performance pin-electronics driver with built-in level-setting DACs, ideal for memory and SOC ATE...
Datasheet
MAX32000 on Analog.com
Hi All, out to.
What is the function of "Low Leak" and "High Imepedance Receive" mode in pin electronics MAX32000 ?
Regards, JJ
Hi JJ,
In MAX32000 "Low Leak" mode, you have the lowest leakage (nA range) at the DUT_ pins and there is essentially no functionality from MAX32000. In "High Impedance Receive", the leakage is higher (uA range) but the comparator, and the OVHV and OVLV (over voltage) are functional.
Hope this answers your question.
Regards,
Hooman
Hi Hooman,
Many thanks for the explanation.
Really very helpful, JJ