Article MAX9979: FAQ Voltage Clamps of Driver

How do I set voltage clamps of driver in MAX9979?

The voltage clamps (high and low) limit the voltage at DUT_. Set the clamp voltages using the level-setting DACs (CPHV_ and CPLV_). Set the clamp voltages at least 0.7V outside the expected DUT_ voltage range when not using the . Driver clamps are always and only enabled in driver high-impedance mode.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.