MAX9979: FAQ

  • Created
Was this helpful?
  • MAX9979: FAQ Driver Operation Range

    What is the driver operation range in MAX9979? Driver operation range in MAX9979 is -2.5V to 6.5V. Refer to to get this information for our various ATE ICs.
  • MAX9979: FAQ Impedance Termination at DUT_pin

    What is impedance termination at DUT_ pin of MAX9979? Nominal output impedance of MAX9979 is 50 ohm. This nominal 50Ω driver output resistance is adjustable by ±2.5Ω with a 360mΩ . This flexibility in…
  • MAX9979: FAQ PMU Functionality

    If the VHH, +13V output is not required, then is it required to provide the +17V VHHP to MAX9979 IC? Can only PMU functionality be utilized without applying +17V to the VHHP pin? Even if super voltage…
  • MAX9979: FAQ Power Dissipation

    What is the power dissipation per channel in MAX9979? Power dissipation per channel in MAX9979 is 1.2W. Refer to to get this information for our various ATE ICs.
  • MAX9979: FAQ Voltage Clamps of Driver

    How do I set voltage clamps of driver in MAX9979 ? The voltage clamps (high and low) limit the voltage at DUT_. Set the clamp voltages using the level-setting DACs (CPHV_ and CPLV_). Set the clamp voltages…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.