Article MAX9972: FAQ Leakage Current

Will the leakage current on one channel of MAX9972 be ‘seen’ on the other driver channels?

Yes. But it is very minimal (in few uA kind of range) and can be reduced to nA range by putting device in low leak mode. That level of leakage would be difficult to separate from the offset, gain, and linearity specifications of the other channels’ Drivers. 

For example, the maximum specified leakage current in Hi-Z mode is 2μA x 50Ω output impedance of one Driver results in 0.1mV of error on the two combined DUT .  Since the DC Characteristic Offset of the MAX9972 drivers is ±10mV Max and the linearity error is about ±0. when driving between -1.0V and +3.0V (see TOC15 on page 9 of the MAX9972 Data Sheet), the leakage current is in the noise when combining one channel in Drive with one channel in Hi-Z.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.