Can the current drive of AD5522 be extended without the use of ganging?
Implementing gang mode to increase the current drive of AD5522 can be a bit tricky due to some factors including the Rsense and path resistance matching. Fortunately, there’s another way to increase the current capability of AD5522 while still possibly enjoying its voltage range, which can be done through cascading an external amplifier through the external current range.

It is important to note that the Rsense may either be adjusted to cater to the larger current drive, or the voltage drop across Rsense may need to be attenuated before going into the measure current circuitry of AD5522 to effectively measure the larger current being driven by external power amplifier.