How accurate can the chip be calibrated to?
As for the accuracy of calibration, zeroing out the offset at the calibration points is achievable but it is always a more proper approach to look at the overall linearity instead, which, according to the datasheet should be better than 0.01% of the full-scale range. Note that this is true for at least the on-chip calibration.

Does it have same accuracy as the system calibration?
Whether on-chip or software system calibration is performed the accuracy of the equipment used to measure these is very important. Any error due to the measurement techniques/equipment will remain post calibration.
In system level calibration, information in data sheet is the guaranteed best range. The error depends to the implementation of customers, how they take their measurements and accuracy of the measuring equipment.