If “Enable Always on Ext Range” is used, how much power consumption is increased?

For AVDD and AVSS, the power consumption for both supplies is increased depending on the load. For example, at 2mA range:
|
Force Voltage |
DUT/Load |
Enable Always on EXT Range @2mA |
Current |
Power |
||||
|
AVDD (15v) |
AVSS (-15V) |
DVCC (+5V) |
AVDD (15v) |
AVSS (-15V) |
DVCC (+5V) |
|||
|
1V |
1kohm |
off |
24mA |
20mA |
2mA |
360mW |
300mW |
10mW |
|
1V |
1kohm |
on |
32mA |
29mA |
2mA |
480mW |
435mW |
10mW |
The following are the values of current displayed using the virtual bench power supply and their corresponding power consumption was computed using the equation P=IV. This is from a 2mA range setting. Please note that the data shown came from a bench test setup with unmodified AD5522 evaluation board.