Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Audio
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Audio
Audio
Documents Why doesn't Analog Devices manufacture 32-bit audio converters?
  • Q&A
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel
  • +Documents
  • +AD1853: FAQ
  • +AD73322: FAQ
  • +AD73311: FAQ
  • +AD73360: FAQ
  • EVAL-SSM2518Z evaluation board documentation and DLL for I2C control
  • Gerber files for Eval board
  • Whether it is pin compatible with TI TPA2010, On-Semi NCP2820?
  • -32-bit Audio Converters: FAQ
    • Why doesn't Analog Devices manufacture 32-bit audio converters?
  • +AD1835: FAQ
  • +AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1852: FAQ
  • +AD1854: FAQ
  • +AD1862: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1881: FAQ
  • +AD1896: FAQ
  • +AD1937: FAQ
  • +ad1938: FAQ
  • +AD1939: FAQ
  • +AD193x: FAQ
  • +AD1955: FAQ
  • +ad1970: FAQ
  • +AD1974: FAQ
  • +AD1981: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +adau1381: FAQ
  • +ADAU1472: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADAU1860: FAQ
  • +ADAU1966: FAQ
  • +ADMP441Z: FAQ
  • +ADMP504: FAQ
  • +CODEC: FAQ
  • +Digital Microphone: FAQ
  • +DS4420: FAQ
  • +EVAL-MICT5818Z: FAQ
  • +HD Audio Codecs: FAQ
  • MAX4063: FAQ
  • +MAX4063ETE+: FAQ
  • +MAX4364ESA+: FAQ
  • +MAX4409ETP+: FAQ
  • +MAX4466EUK: FAQ
  • +MAX4469EKA+: FAQ
  • +MAX5407: FAQ
  • +MAX9709EVKIT: FAQ
  • +MAX9720AEUE+: FAQ
  • +MAX97220AETE+: FAQ
  • MAX9722A: FAQ
  • +MAX9722AETE+: FAQ
  • +MAX9723: FAQ
  • +MAX9730ETI+: FAQ
  • MAX9737ETG+: FAQ
  • +MAX9737ETG+T: FAQ
  • +MAX9738EWP+G45: FAQ
  • +MAX9742ETX+: FAQ
  • MAX9744: FAQ
  • +MAX9744ETH+: FAQ
  • +MAX9759: FAQ
  • +MAX9768BETG+T: FAQ
  • +MAX9788ETI+: FAQ
  • MAX9814: FAQ
  • +MAX9814EBC+T: FAQ
  • +MAX9814ETD+T: FAQ
  • +MAX98300: FAQ
  • +MAX98306ETD+: FAQ
  • MAX98307: FAQ
  • +MAX98307ETE+: FAQ
  • +MAX98307ETE/V+: FAQ
  • MAX98357A: FAQ
  • +MAX98357ADEV#TQFN: FAQ
  • MAX98357AETE+: FAQ
  • +MAX98357AETE+T: FAQ
  • +MAX98357AEWL+T: FAQ
  • +MAX98357BETE+: FAQ
  • +MAX98358EVSYS#WLP: FAQ
  • +MAX98360AENL+T: FAQ
  • +MAX98365AEWC+: FAQ
  • MAX98372: FAQ
  • +MAX98372ETJ+: FAQ
  • +MAX98374EFF+: FAQ
  • +MAX98380: FAQ
  • +MAX98390CEWX+T: FAQ
  • +MAX98390EVSYS#: FAQ
  • MAX98390EWX+: FAQ
  • +MAX98390EWX+T: FAQ
  • +MAX98395EVSYS#: FAQ
  • +MAX98395EWG+: FAQ
  • +MAX98396EVSYS#: FAQ
  • +MAX98396EWB+: FAQ
  • +MAX98400BETG+: FAQ
  • +MAX98500EWE+: FAQ
  • +MAX9850EVKIT#: FAQ
  • +MAX98927EWX+: FAQ
  • +MEMS mics: FAQ
  • +Power supplies, capacitors, and application schematics: FAQ
  • REGEN and THERM: FAQ
  • +SigmaStudio: FAQ
  • +ssm2166: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2306: FAQ
  • ssm2311: FAQ
  • +SSM2315: FAQ
  • +SSM2380: FAQ
  • ssm2518: FAQ
  • +SSM2529: FAQ
  • +ssm2602: FAQ
  • +SSM2603: FAQ
  • +SSM3302: FAQ

Why doesn't Analog Devices manufacture 32-bit audio converters?

Several customers have asked lately if Analog Devices has any 32-bit audio converters in our product offering. At the moment, we do not. The reasoning for this is as follows:

A 24-bit converter has a theoretical noise floor of -144 dBFS (that is, relative to the full scale signal level), but in practice, a converter (ADC or DAC) never achieves that high performance. The very best converters on the market right now for 3.3 V audio systems only make use of about 22 bits (with the bottom 2 bits sitting in the noise floor of the converter) giving an effective noise floor of around -132 dB. Most cost-competitive converters have noise floors in the -100 dB to -120 dB range. Once the audio signal is in the analog domain, the 3.3 V full-scale signal path (consiting of PCB traces, resistors, capacitors, and op amps) has a practical noise floor of slightly below -130 dB. This residual environmental noise is due to natural factors like solar radiation, thermal noise, radio waves, and other "natural" sources of noise.

Some 32-bit converters are now available on the market, but in reality, the analog performance of these converters, and the environmental noise in the system, are still the gating factors of the overall system performance. Only about 22 bits carry signal and the remaining 10 bits are simply lost due to the noise floor of the "weak links" in the signal chain. So, it can be argued that having a 32-bit converter in a 3.3 V audio system is really not adding any value compared to what a 24-bit converter would do, at least when the performance limits of current converter technology are taken into consideration.

There is, however, some merit to having a 32-bit DSP core in an audio system, because calculations done in the digital realm are subject to quantization noise and minor calculation errors. For that reason, it can be worthwhile to have a 32-bit DSP core surrounded by 24-bit audio converters (with dither performed during the bit depth conversion stage of the system).