Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Audio
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Audio
Audio
Documents AD1937: Failure due to  I2C interface
  • Q&A
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel

Products Mentioned

AD1937 Production
The AD1937 is a high performance, single-chip codec that provides four analog-to-digital converters (ADCs) with differential input and eight digital-to...
Datasheet
AD1937 on Analog.com

  • +Documents
  • +AD1853: FAQ
  • +AD73322: FAQ
  • +AD73311: FAQ
  • +AD73360: FAQ
  • EVAL-SSM2518Z evaluation board documentation and DLL for I2C control
  • Gerber files for Eval board
  • Whether it is pin compatible with TI TPA2010, On-Semi NCP2820?
  • +32-bit Audio Converters: FAQ
  • +AD1835: FAQ
  • +AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1852: FAQ
  • +AD1854: FAQ
  • +AD1862: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1881: FAQ
  • +AD1896: FAQ
  • -AD1937: FAQ
    • AD1937: Failure due to  I2C interface
  • +ad1938: FAQ
  • +AD1939: FAQ
  • +AD193x: FAQ
  • +AD1955: FAQ
  • +ad1970: FAQ
  • +AD1974: FAQ
  • +AD1981: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +adau1381: FAQ
  • +ADAU1472: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADAU1860: FAQ
  • +ADAU1966: FAQ
  • +ADMP441Z: FAQ
  • +ADMP504: FAQ
  • +CODEC: FAQ
  • +Digital Microphone: FAQ
  • +DS4420: FAQ
  • +EVAL-MICT5818Z: FAQ
  • +HD Audio Codecs: FAQ
  • MAX4063: FAQ
  • +MAX4063ETE+: FAQ
  • +MAX4364ESA+: FAQ
  • +MAX4409ETP+: FAQ
  • +MAX4466EUK: FAQ
  • +MAX4469EKA+: FAQ
  • +MAX5407: FAQ
  • +MAX9709EVKIT: FAQ
  • +MAX9720AEUE+: FAQ
  • +MAX97220AETE+: FAQ
  • MAX9722A: FAQ
  • +MAX9722AETE+: FAQ
  • +MAX9723: FAQ
  • +MAX9730ETI+: FAQ
  • MAX9737ETG+: FAQ
  • +MAX9737ETG+T: FAQ
  • +MAX9738EWP+G45: FAQ
  • +MAX9742ETX+: FAQ
  • MAX9744: FAQ
  • +MAX9744ETH+: FAQ
  • +MAX9759: FAQ
  • +MAX9768BETG+T: FAQ
  • +MAX9788ETI+: FAQ
  • MAX9814: FAQ
  • +MAX9814EBC+T: FAQ
  • +MAX9814ETD+T: FAQ
  • +MAX98300: FAQ
  • +MAX98306ETD+: FAQ
  • MAX98307: FAQ
  • +MAX98307ETE+: FAQ
  • +MAX98307ETE/V+: FAQ
  • MAX98357A: FAQ
  • +MAX98357ADEV#TQFN: FAQ
  • MAX98357AETE+: FAQ
  • +MAX98357AETE+T: FAQ
  • +MAX98357AEWL+T: FAQ
  • +MAX98357BETE+: FAQ
  • +MAX98358EVSYS#WLP: FAQ
  • +MAX98360AENL+T: FAQ
  • +MAX98365AEWC+: FAQ
  • MAX98372: FAQ
  • +MAX98372ETJ+: FAQ
  • +MAX98374EFF+: FAQ
  • +MAX98380: FAQ
  • +MAX98390CEWX+T: FAQ
  • +MAX98390EVSYS#: FAQ
  • MAX98390EWX+: FAQ
  • +MAX98390EWX+T: FAQ
  • +MAX98395EVSYS#: FAQ
  • +MAX98395EWG+: FAQ
  • +MAX98396EVSYS#: FAQ
  • +MAX98396EWB+: FAQ
  • +MAX98400BETG+: FAQ
  • +MAX98500EWE+: FAQ
  • +MAX9850EVKIT#: FAQ
  • +MAX98927EWX+: FAQ
  • +MEMS mics: FAQ
  • +Power supplies, capacitors, and application schematics: FAQ
  • REGEN and THERM: FAQ
  • +SigmaStudio: FAQ
  • +ssm2166: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2306: FAQ
  • ssm2311: FAQ
  • +SSM2315: FAQ
  • +SSM2380: FAQ
  • ssm2518: FAQ
  • +SSM2529: FAQ
  • +ssm2602: FAQ
  • +SSM2603: FAQ
  • +SSM3302: FAQ

AD1937: Failure due to  I2C interface

Q 

We have an audio device built around the ADAU1445-DSP and the AD1937 CODEC. 
The ADAU1445-DSP is the clock master.
Both of them are controlled on the same I2C bus by a processor, with a
software, (‘bit bang’), I2C.
7 bit address of the AD1937 is 0x04 and the ADAU1445 is 0x38.
When our processor gets busy, the I2C is a low priority and gets interrupted.
We can see on the oscilloscope that sometimes midway through an I2C
transaction, both the SCL and the SDA ports stay low for about 40ms.
This within the I2C specs as there’s no limit on clock or data speed, the I2C
protocol analyzer, (http://www.totalphase.com/products/beagle_ism/ ),  shown no
errors, took us a while to notice the 40ms delay in the transaction.
When this 40ms both signal low happens, the AD1937’s AD clocks lock up:
- Both clock pins, (ALRCLK and ALRCLK), turn from normally configured input to
output,
(and as our system is normally configured as CODEC slave, we have very loud
noise sent on all AD channels with two out of phase clock sources).
- I2C communication is working OK, can write and read all registers.
- Verified, that all written commands into registers are correctly executed,
except the AD clock pin directions, we can even change the ABCLK rate.
Only Hardware reset will release the AD1937 from this locked state.   We are
wondering if this problem is known to AD, or you can see something we are
missing, (and possibly on the wrong track).

 

A 

We have done a comprehensive analysis of Stand Alone mode in the AD193x family
of parts. Given the fact that the customer is using the AD1937, I will refer to
the I2C pins, with respect to the corresponding stand alone mode pins.

There are 4 pins total that are used for Stand Alone mode: ADDR0, ADDR1, SCL,
and SDA, see the table 12 n the datasheet.

Usually, it would be assumed that an IC would look at the Stand Alone mode port
once at startup and stay fixed, in or out, of Stand Alone mode until the next
reset. However, it appears from bench testing that the AD1937 will go into
Stand Alone mode if ADDR0, ADDR1 and SCL are all held Low for more than 4 mS,
with the state of SDA setting the ADC Clock ports to Master or Slave. At the
same time, the Stand Alone mode will revert to *default* state if the pin
conditions above are removed.
If the customer is using ADDR 00, two of the three pins are already low. If the
SDA and SCL pins are held low for 40 mS, this would certainly put the part in
Stand Alone Slave mode, and when the SDA and SCL pins come back high, the part
will be left in default. The easiest solution would be to change the I2C
address by pulling either or both ADDR0/1 pins high; the AD1937 will never go
into Stand Alone mode.
P.S. After some lengthy testing, it turns out that the part does not lose its
register settings when it goes into and comes out of Stand Alone mode.

Tags: ad1937