Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Audio
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Audio
Audio
Documents AD1939
  • Q&A
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel

Products Mentioned

AD1939 Production
The AD1939 is a high performance, single-chip codec that provides four analog-to-digital converters (ADCs) with differential input, and eight digital-to...
Datasheet
AD1939 on Analog.com

  • +Documents
  • +AD1853: FAQ
  • +AD73322: FAQ
  • +AD73311: FAQ
  • +AD73360: FAQ
  • EVAL-SSM2518Z evaluation board documentation and DLL for I2C control
  • Gerber files for Eval board
  • Whether it is pin compatible with TI TPA2010, On-Semi NCP2820?
  • +32-bit Audio Converters: FAQ
  • +AD1835: FAQ
  • +AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1852: FAQ
  • +AD1854: FAQ
  • +AD1862: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1881: FAQ
  • +AD1896: FAQ
  • +AD1937: FAQ
  • +ad1938: FAQ
  • -AD1939: FAQ
    • AD1939
    • AD1939: datasheet contradictions on SPI timing specification
    • Request for a 32 bit audio codec
  • +AD193x: FAQ
  • +AD1955: FAQ
  • +ad1970: FAQ
  • +AD1974: FAQ
  • +AD1981: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +adau1381: FAQ
  • +ADAU1472: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADAU1860: FAQ
  • +ADAU1966: FAQ
  • +ADMP441Z: FAQ
  • +ADMP504: FAQ
  • +CODEC: FAQ
  • +Digital Microphone: FAQ
  • +DS4420: FAQ
  • +EVAL-MICT5818Z: FAQ
  • +HD Audio Codecs: FAQ
  • MAX4063: FAQ
  • +MAX4063ETE+: FAQ
  • +MAX4364ESA+: FAQ
  • +MAX4409ETP+: FAQ
  • +MAX4466EUK: FAQ
  • +MAX4469EKA+: FAQ
  • +MAX5407: FAQ
  • +MAX9709EVKIT: FAQ
  • +MAX9720AEUE+: FAQ
  • +MAX97220AETE+: FAQ
  • MAX9722A: FAQ
  • +MAX9722AETE+: FAQ
  • +MAX9723: FAQ
  • +MAX9730ETI+: FAQ
  • MAX9737ETG+: FAQ
  • +MAX9737ETG+T: FAQ
  • +MAX9738EWP+G45: FAQ
  • +MAX9742ETX+: FAQ
  • MAX9744: FAQ
  • +MAX9744ETH+: FAQ
  • +MAX9759: FAQ
  • +MAX9768BETG+T: FAQ
  • +MAX9788ETI+: FAQ
  • MAX9814: FAQ
  • +MAX9814EBC+T: FAQ
  • +MAX9814ETD+T: FAQ
  • +MAX98300: FAQ
  • +MAX98306ETD+: FAQ
  • MAX98307: FAQ
  • +MAX98307ETE+: FAQ
  • +MAX98307ETE/V+: FAQ
  • MAX98357A: FAQ
  • +MAX98357ADEV#TQFN: FAQ
  • MAX98357AETE+: FAQ
  • +MAX98357AETE+T: FAQ
  • +MAX98357AEWL+T: FAQ
  • +MAX98357BETE+: FAQ
  • +MAX98358EVSYS#WLP: FAQ
  • +MAX98360AENL+T: FAQ
  • +MAX98365AEWC+: FAQ
  • MAX98372: FAQ
  • +MAX98372ETJ+: FAQ
  • +MAX98374EFF+: FAQ
  • +MAX98380: FAQ
  • +MAX98390CEWX+T: FAQ
  • +MAX98390EVSYS#: FAQ
  • MAX98390EWX+: FAQ
  • +MAX98390EWX+T: FAQ
  • +MAX98395EVSYS#: FAQ
  • +MAX98395EWG+: FAQ
  • +MAX98396EVSYS#: FAQ
  • +MAX98396EWB+: FAQ
  • +MAX98400BETG+: FAQ
  • +MAX98500EWE+: FAQ
  • +MAX9850EVKIT#: FAQ
  • +MAX98927EWX+: FAQ
  • +MEMS mics: FAQ
  • +Power supplies, capacitors, and application schematics: FAQ
  • REGEN and THERM: FAQ
  • +SigmaStudio: FAQ
  • +ssm2166: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2306: FAQ
  • ssm2311: FAQ
  • +SSM2315: FAQ
  • +SSM2380: FAQ
  • ssm2518: FAQ
  • +SSM2529: FAQ
  • +ssm2602: FAQ
  • +SSM2603: FAQ
  • +SSM3302: FAQ

AD1939

Q 

Please clarify how the AD1939 decides between Standalone and SPI mode.

 

A 

As described in the Serial Control Port section on page 14 of the datasheet,
powering up the AD1939 in Stand Alone mode puts the part in default mode with
the exception of the Internal MCLK Enable bit which comes up enabled (Register
0x00 [7]). This would be defined as 256×fs, I2S stereo, MCLK PLL, 32 kHz – 48
kHz fs window. In Stand Alone Mode, there is no SPI control over the AD1939
until the part is reset by power cycling or toggling the reset pin.
The part is put in Stand Alone mode by holding the CIN (pin 30), CCLK (pin 34),
and CLATCH (pin 35) low at powerup. As shown in Table 11, the state of the COUT
(pin 31) at powerup sets the ADC LRCLK and BCLK ports to be either Master
(output) or Slave (input). This does not have any impact on the SPI comm port
that sets the registers for the AD1939.
Table 11 shows the required state of the 4 SPI port pins to put the AD1939 in
either of the two possible Stand Alone modes.
The AD1939 is always and only a SPI Slave. It cannot act as a SPI Master. The
Master and Slave references are to the ADC clocks, as shown in Table 11.
The Automated Register Window Builder is an application that we have written to
control the AD1939 and other codec products within DAU; it is available on the
AD1939 product page under ‘Tools, Software & Sim Models.’ In conjunction with
our USB interface (EVAL-ADUSB2EBZ), Honeywell should be able to see the
conversation between the software and the AD1939.

Tags: ad1939