Q
The datasheet of AD73360 gives typical values only for some of the
parameters.The information is back from 2000. Perhaps some min or max values
have become available in the mean time which you can make available to me? I am
interested in long term drift of UREF, long term drift of gain, minmax values
for the frequency response and the FIT in particular. These long term data
might have helped to set up a maintenance plan which is badly needed because
our instruments are expected to stay in service substantially in excess of
10years.
Operating conditions:I am supplying AD73360 with 5Volts at AVD and 3.3Volts at
DVD
A
Long term drift specifications are especially very difficult to come up with,
so sorry the answer is no, we do not have any additional specifications for
these parameters other those provided in the datasheet.
With regards to FIT:
For reliability information, the MTTF and FIT results based on HTOL (High
Temperature Operating Lifetest)for our parts is available on the Internet at
the following URL:
http://www.analog.com/en/content/Quality-Reliability/fca.html
Follow these steps:
- Select "Reliability Program" link
- Select "Wafer Fab Process Data"
- Select product under "PRODUCT P/N"(for example: AD73360)from drop down menu
- Click on Submit button.
See the Process Technology Life test data summary table for FIT rate, MTTF etc.