Analog.com
Analog
Dialogue
Wiki
English
Analog.com
Analog
Dialogue
Wiki
简体中文
EngineerZone
Site
Search
User
Site
Search
User
EngineerZone
Search
Log in
Site
Search
Log in
Home
Blogs ⌵
EngineerZone Spotlight
The Engineering Mind
Browse ⌵
All Groups
All Members
Support ⌵
3D ToF Depth Sensing
Amplifiers
Analog Microcontrollers
Audio
Clock and Timing
Data Converters
Design Tools and Calculators
Direct Digital Synthesis (DDS)
Embedded Vision Sensing
Energy Monitoring and Metering
FPGA Reference Designs
Industrial Ethernet
Interface and Isolation
Low Power RF Transceivers
MEMS Inertial Sensors
Motor Control Hardware Platforms
Optical Sensing
Power By Linear
Processors and DSP
Reference Circuits
RF and Microwave
Switches/Multiplexers
Temperature Sensors
Video
Wide Band RF Transceivers
Wireless Sensor Networks Reference Library
My EZ
More
Cancel
主页
浏览 ⌵
收件箱
个人设置
会员
专区列表
论坛专区 ⌵
放大器专区
精密转换器专区
音频专区
ADE电能计量专区
MEMS和传感器专区
接口和隔离专区
Power 中文专区
ADUC微处理器专区
锁相环专区
开关和多路复用器专区
温度传感器
基准电压源专区
资源库
论坛使用指南
技术支持参考库
在线研讨会
论坛社群活动
论坛激励活动
More
Cancel
Audio
Documents
AD73360: Reference voltage
Q&A
Discussions
Documents
File Uploads
Video/Images
Tags
Managers
More
Cancel
New
Audio requires membership for participation - click to join
+
Documents
"quad-buffer" headphone amplifier
AD1835: Output filters
AD1835A: DC offset voltage
AD1836: Sampling at 22.05kHz
AD1845: DC offset
AD1852: ESD sensitivity, HBM model data missing from datasheet
AD1853 EVB
AD1853: output impedance
AD1853: Two devices in parallel
AD1854: SPI port unused
AD1862
AD1871 single ended input range
AD1877: Calculation of the LSB value
AD1896: Configuration
AD1937: Failure due to I2C interface
AD1939
AD1939: datasheet contradictions on SPI timing specification
AD193x family - supporting Sample Rates lower than 32 kHz
AD1955: Independency of the channels
AD1974 Stop Band Filter Response
AD1981 PCB Layout recommendation
AD1981B drivers
AD1981B EVB
AD1986: AC97 code
AD1992: Driving the input stage
AD73311: Power supply
AD73311: Power supply sequencing problem, using DVDD = 3.3V and AVDD = 5.2V
AD73311L: Cascade running at different sampling speeds
AD73322/AD73322L compatibility
AD73322: CD measurability
AD73322: Vref transfer function
AD73322L: Frequency response
AD73360 timing questions
AD73360: Frequency response over sample rate
AD73360: Grounding
AD73360: Lower limit of the MCLK
AD73360: Reference voltage
AD73360: SDOFS in figure 10
AD73360: Settling time when changing the PGA gain
AD73360AR: DC performance
AD73360L: Reference does not always power up
ADAU1761: Can I connect one analog and one digital input channel to the ADAU1761 and process both of them together?
ADAU1966 maximum load current
ADAU1966: If using a direct MCLK can I leave LF and PLLVDD pins disconnected?
AVDD and DVDD range
Binary 2.20 format
Can AD1836A work at 32KHz or 44.1KHz sample rate?
Change sample rate by controlling SE pin.
Clicks and pops on power up
Dejitter issue
Do Analog Devices still have a range of HD Audio Codecs or has this technology all been sold off to Conexant?
Does the AD1852 accept SPDIF format?
Does volume control setting affect THD+N ?
EVAL-ADAU1472Z Evaluation Board support files (public)
EVAL-SSM2518Z evaluation board documentation and DLL for I2C control
Evaluation board Datasheet
FAQ: Can a digital microphone's PDM output be directly connected to an I2S input?
FAQ: Can MEMS mics be soldered to a flex PCB?
FAQ: Is a microphone with higher sensitivity better than one with lower sensitivity?
Gerber files for Eval board
How do I handle unused digital pins on an AD193x codec?
How to connect unused SDATA inputs on ADAU1966?
How to create an EEPROM image for the ADAU1772 that has different filter coefficients in Bank A and Bank B
I2S interface configuration
Interesting microphone application - "Acoustic telescope"
Long term drift for gain, Uref and FIT data
Low latency audio codec
MEMS microphone IBIS models
New MEMS microphone products
Power supplies, capacitors, and application schematics
Ref out voltage of the EVB
REGEN and THERM pins
Replacement for WM8731SEFL
Request for a 32 bit audio codec
Sample rate lower than 32KHz
SigmaStudio Help File - where could I find it
SSM2250: Replacement type available?
SSM2302: Output overshoot.
SSM2306: Exposed pad connection
SSM2529 Evaluation Board Documentation
SSM2529: Evaluation board documentation
SSM2603 audio codec power supply questions
SSM2603/SSM2604 Boot Sequence
Stand-alone Modes on the AD193x audio CODECs
Temperature drift of the internal PGA
The relationship between value of Input Level Control register (Address 0) and gain value
Unused analog input pin connection
Using ADAU1761 for microphone beamforming
Using ADAU1772 for microphone beamforming
Using LRCLK as PLL input
Video: Getting started with the EVAL-ADMP441Z
Video: Microphone Array Beamforming with the ADMP504
Whether it is pin compatible with TI TPA2010, On-Semi NCP2820?
Why doesn't Analog Devices manufacture 32-bit audio converters?
Working at 8KHz sample rate
AD73360: Reference voltage
Q
I am using the DC coupled configuration in which VINN is shorted to VREFOUT of
1.25V and the input voltage is applied to VINPX (Fig. 27). What is the voltage
range on VINPX and LSB value in millivolts?
A
The data sheet gives 1.64375Vp-p input voltage (measured differentially). This
means the absolute voltage input has to account for the 1.25V reference:
1.25+/-1.64375/2 V for Figure 27 configuration
As for the LSB value, the bottom transfer function of Figure 8 (single ended)
should be used because Vref*0.6575=1.64375/2. Then, the digital output is
function of Data Mode/Mixed Mode bits: 16 or 15 bits.
ad73360
Share
History
More
Cancel
Comments
Related