Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Dont Let Your Feedback Loop Fall FlatPart 2: Dynamic Response and Isolation Innovation!

    Introduction In isolated power supply systems, maintaining a stable output voltage under varying load conditions is essential for reliable operation. The...

EngineerZone
EngineerZone
Audio
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Audio
Audio
Documents Can the left and right output channels of the MAX98306 be joined together?
  • Q&A
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel

Products Mentioned

MAX98306 Production
The MAX98306 stereo 3.7W Class D amplifier provides Class AB audio performance with Class D efficiency. This device offers five selectable gain settings...
Datasheet
MAX98306 on Analog.com

  • +Documents
  • +AD1853: FAQ
  • +AD73322: FAQ
  • +AD73311: FAQ
  • +AD73360: FAQ
  • EVAL-SSM2518Z evaluation board documentation and DLL for I2C control
  • Gerber files for Eval board
  • Whether it is pin compatible with TI TPA2010, On-Semi NCP2820?
  • +32-bit Audio Converters: FAQ
  • +AD1835: FAQ
  • +AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1852: FAQ
  • +AD1854: FAQ
  • +AD1862: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1881: FAQ
  • +AD1896: FAQ
  • +AD1937: FAQ
  • +ad1938: FAQ
  • +AD1939: FAQ
  • +AD193x: FAQ
  • +AD1955: FAQ
  • +ad1970: FAQ
  • +AD1974: FAQ
  • +AD1981: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +adau1381: FAQ
  • +ADAU1472: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADAU1860: FAQ
  • +ADAU1966: FAQ
  • +ADMP441Z: FAQ
  • +ADMP504: FAQ
  • +CODEC: FAQ
  • +Digital Microphone: FAQ
  • +DS4420: FAQ
  • +EVAL-MICT5818Z: FAQ
  • +HD Audio Codecs: FAQ
  • MAX4063: FAQ
  • +MAX4063ETE+: FAQ
  • +MAX4364ESA+: FAQ
  • +MAX4409ETP+: FAQ
  • +MAX4466EUK: FAQ
  • +MAX4469EKA+: FAQ
  • +MAX5407: FAQ
  • +MAX9709EVKIT: FAQ
  • +MAX9720AEUE+: FAQ
  • +MAX97220AETE+: FAQ
  • MAX9722A: FAQ
  • +MAX9722AETE+: FAQ
  • +MAX9723: FAQ
  • +MAX9730ETI+: FAQ
  • MAX9737ETG+: FAQ
  • +MAX9737ETG+T: FAQ
  • +MAX9738EWP+G45: FAQ
  • +MAX9742ETX+: FAQ
  • MAX9744: FAQ
  • +MAX9744ETH+: FAQ
  • +MAX9759: FAQ
  • +MAX9768BETG+T: FAQ
  • +MAX9788ETI+: FAQ
  • MAX9814: FAQ
  • +MAX9814EBC+T: FAQ
  • +MAX9814ETD+T: FAQ
  • +MAX98300: FAQ
  • -MAX98306ETD+: FAQ
    • Can the left and right output channels of the MAX98306 be joined together?
    • Does the MAMX98306 have a slew rate specification for EMI considerations?
  • MAX98307: FAQ
  • +MAX98307ETE+: FAQ
  • +MAX98307ETE/V+: FAQ
  • MAX98357A: FAQ
  • +MAX98357ADEV#TQFN: FAQ
  • MAX98357AETE+: FAQ
  • +MAX98357AETE+T: FAQ
  • +MAX98357AEWL+T: FAQ
  • +MAX98357BETE+: FAQ
  • +MAX98358EVSYS#WLP: FAQ
  • +MAX98360AENL+T: FAQ
  • +MAX98365AEWC+: FAQ
  • MAX98372: FAQ
  • +MAX98372ETJ+: FAQ
  • +MAX98374EFF+: FAQ
  • +MAX98380: FAQ
  • +MAX98390CEWX+T: FAQ
  • +MAX98390EVSYS#: FAQ
  • MAX98390EWX+: FAQ
  • +MAX98390EWX+T: FAQ
  • +MAX98395EVSYS#: FAQ
  • +MAX98395EWG+: FAQ
  • +MAX98396EVSYS#: FAQ
  • +MAX98396EWB+: FAQ
  • +MAX98400BETG+: FAQ
  • +MAX98500EWE+: FAQ
  • +MAX9850EVKIT#: FAQ
  • +MAX98927EWX+: FAQ
  • +MEMS mics: FAQ
  • +Power supplies, capacitors, and application schematics: FAQ
  • REGEN and THERM: FAQ
  • +SigmaStudio: FAQ
  • +ssm2166: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2306: FAQ
  • ssm2311: FAQ
  • +SSM2315: FAQ
  • +SSM2380: FAQ
  • ssm2518: FAQ
  • +SSM2529: FAQ
  • +ssm2602: FAQ
  • +SSM2603: FAQ
  • +SSM3302: FAQ

Can the left and right output channels of the MAX98306 be joined together?

It is possible to tie the left and right outputs together only if the left and right inputs are tied together also. This does not eliminate the possibility of shoot through in the internal MOSFETs however. If shoot through does occur a large current spike will likely destroy the IC, this current can be limited by adding series resistance between the tied outputs but care must be taken to choose a suitable power rating for the resistors.

Tags: Audio Products KA-07975 joined together MAX98306 Audio Amplifiers common connection MAX98306ETD+ Show More