Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Audio
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Audio
Audio
Documents How can one estimate the input supply current of the MAX97220 audio amplifier ?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

MAX97220A Production
The MAX97220 is a differential input DirectDrive® line driver/headphone amplifier. This device is capable of driving line level loads with 3VRMS into...
Datasheet
MAX97220A on Analog.com

MAX97220B Production
The MAX97220 is a differential input DirectDrive® line driver/headphone amplifier. This device is capable of driving line level loads with 3VRMS into...
Datasheet
MAX97220B on Analog.com

MAX97220E Production
The MAX97220 is a differential input DirectDrive® line driver/headphone amplifier. This device is capable of driving line level loads with 3VRMS into...
Datasheet
MAX97220E on Analog.com

MAX97220D Production
The MAX97220 is a differential input DirectDrive® line driver/headphone amplifier. This device is capable of driving line level loads with 3VRMS into...
Datasheet
MAX97220D on Analog.com

MAX97220C Production
The MAX97220 is a differential input DirectDrive® line driver/headphone amplifier. This device is capable of driving line level loads with 3VRMS into...
Datasheet
MAX97220C on Analog.com

  • +Documents
  • +AD1853: FAQ
  • +AD73322: FAQ
  • +AD73311: FAQ
  • +AD73360: FAQ
  • EVAL-SSM2518Z evaluation board documentation and DLL for I2C control
  • Gerber files for Eval board
  • Whether it is pin compatible with TI TPA2010, On-Semi NCP2820?
  • +32-bit Audio Converters: FAQ
  • +AD1835: FAQ
  • +AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1852: FAQ
  • +AD1854: FAQ
  • +AD1862: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1881: FAQ
  • +AD1896: FAQ
  • +AD1937: FAQ
  • +ad1938: FAQ
  • +AD1939: FAQ
  • +AD193x: FAQ
  • +AD1955: FAQ
  • +ad1970: FAQ
  • +AD1974: FAQ
  • +AD1981: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +adau1381: FAQ
  • +ADAU1472: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADAU1860-1: FAQ
  • +ADAU1966: FAQ
  • +ADMP441Z: FAQ
  • +ADMP504: FAQ
  • +CODEC: FAQ
  • +Digital Microphone: FAQ
  • +DS4420: FAQ
  • +EVAL-MICT5818Z: FAQ
  • +HD Audio Codecs: FAQ
  • MAX4063: FAQ
  • +MAX4063ETE+: FAQ
  • +MAX4364ESA+: FAQ
  • +MAX4409ETP+: FAQ
  • +MAX4466EUK: FAQ
  • +MAX4469EKA+: FAQ
  • +MAX5407: FAQ
  • +MAX9709EVKIT: FAQ
  • +MAX9720AEUE+: FAQ
  • -MAX97220AETE+: FAQ
    • Do the outputs of MAX97220 sink current when the supply voltage is not present ?
    • Has Maxim performed any destructive testing on the MAX97220AETE+ devices?
    • How can I determine if the MAX97220 encounters a thermal-overload event?
    • How can one estimate the input supply current of the MAX97220 audio amplifier ?
    • Is MAX97220A Compatible with MAX9722 in Non-Differential Mode?
    • What is the recommended minimum load (RL) for the MAX97220A?
    • What's the difference between MAX97220A and MAX97220C?
  • MAX9722A: FAQ
  • +MAX9722AETE+: FAQ
  • +MAX9723: FAQ
  • +MAX9730ETI+: FAQ
  • MAX9737ETG+: FAQ
  • +MAX9737ETG+T: FAQ
  • +MAX9738EWP+G45: FAQ
  • +MAX9742ETX+: FAQ
  • MAX9744: FAQ
  • +MAX9744ETH+: FAQ
  • +MAX9759: FAQ
  • +MAX9768BETG+T: FAQ
  • +MAX9788ETI+: FAQ
  • MAX9814: FAQ
  • +MAX9814EBC+T: FAQ
  • +MAX9814ETD+T: FAQ
  • +MAX98300: FAQ
  • +MAX98306ETD+: FAQ
  • MAX98307: FAQ
  • +MAX98307ETE+: FAQ
  • +MAX98307ETE/V+: FAQ
  • MAX98357A: FAQ
  • +MAX98357ADEV#TQFN: FAQ
  • MAX98357AETE+: FAQ
  • +MAX98357AETE+T: FAQ
  • +MAX98357AEWL+T: FAQ
  • +MAX98357BETE+: FAQ
  • +MAX98358EVSYS#WLP: FAQ
  • +MAX98360AENL+T: FAQ
  • +MAX98365AEWC+: FAQ
  • MAX98372: FAQ
  • +MAX98372ETJ+: FAQ
  • +MAX98374EFF+: FAQ
  • +MAX98380: FAQ
  • +MAX98390CEWX+T: FAQ
  • +MAX98390EVSYS#: FAQ
  • MAX98390EWX+: FAQ
  • +MAX98390EWX+T: FAQ
  • +MAX98395EVSYS#: FAQ
  • +MAX98395EWG+: FAQ
  • +MAX98396EVSYS#: FAQ
  • +MAX98396EWB+: FAQ
  • +MAX98400BETG+: FAQ
  • +MAX98500EWE+: FAQ
  • +MAX9850EVKIT#: FAQ
  • +MAX98927EWX+: FAQ
  • +MEMS mics: FAQ
  • +Power supplies, capacitors, and application schematics: FAQ
  • REGEN and THERM: FAQ
  • +SigmaStudio: FAQ
  • +ssm2166: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2306: FAQ
  • ssm2311: FAQ
  • +SSM2315: FAQ
  • +SSM2380: FAQ
  • ssm2518: FAQ
  • +SSM2529: FAQ
  • +ssm2602: FAQ
  • +SSM2603: FAQ
  • +SSM3302: FAQ

How can one estimate the input supply current of the MAX97220 audio amplifier ?

If the audio output power (Pout) of the MAX97220 audio amplifier is known, the input power (Pin) can be calculated as : 

Pin = Pout + Pd

where,

Pin = Power supplied to the audio amp

Pout = Output power of the audio amp

Pd = Power Dissipation of the audio amp

Power Dissipation can be determined from the datasheet typical operating characteristic Power Dissipation vs. Output Power (toc22).

 For example, for an output power of  125mW per channel, the power dissipation is 350 mW. 

Pd = 350mW

Since 125mW is output power per channel,  Pout = 2x125mW  = 250mW

 

Pin = 250mW + 350mW =   600 mW

 

If Vin = 5V (supply voltage) , since  Pin = Vin x Iin,

Iin = 600/5 = 120mA (supply current) .

Tags: output power product KA-04858 MAX97220AETE+ supply current audio amplifier MAX97220 power supply Show More