Hi All.
I am designing a low power audio system with the intention of using an ADAU1777 with a MAX98390.
I notice the ADAU1777 has only one serial port but I was unsure if it could support full duplex on I2S for input to the ADAU and then output to the MAX98390 from the ADAU1777 or if it could do I2S input, and then TDM output on the 7 available MPx pins.
Many Thanks!