Post Go back to editing

How to generate HEX file for selfboot

Category: Hardware
Product Number: ADAU1860

Hello,

I have a question on "burning" Flash for ADAU1860. How to generate HEX file for  the flash burn (or writing the program to Flash device)? I need to power up the ADAU1860 with "Selfboot mode" or "Flash boot method".

It worked fine to boot it in "SRAM boot method" with the hex file produced by the following command and reset it with 0x60000400:

xt-dumpelf.exe --base=0x60000000 --width=32 --full --size=0x30000 --little-endian mybinfile > program.hex

but the same hex file does not work with "unpacked selfboot mode".

Regards,

Choe

  • Hello Choe,

    The addresses for Flash vs SRAM boot are different, so you need to change your memory map accordingly and regenerate the linker scripts with xt-genldscripts. Here you can see an example of memmap.xmm for use with flash boot:

    ROMING=true
    VECSELECT=1
    VECRESET=0x68000000
    
    BEGIN srom
    0x68000000: sysrom : srom : 0x30000 : executable ;
     srom0 : F : 0x68000000 - 0x6802ffff : .ResetVector.text .ResetHandler.literal .ResetHandler.text .srom.rodata .srom.literal .srom.text .rom.store;
    END srom
    
    BEGIN dram0
    0x5fff0000: dataRam : dram0 : 0x4000 : writable ;
     dram0_0 : C : 0x5fff0000 - 0x5fff3fff : .dram0.rodata .dram0.literal .dram0.data .dram0.bss;
    END dram0
    
    BEGIN dram1
    0x5fff4000: dataRam : dram1 : 0x4000 : writable ;
     dram1_0 : C : 0x5fff4000 - 0x5fff7fff : .dram1.rodata .iram0.literal .dram1.literal .dram1.data .dram1.bss;
    END dram1
    
    BEGIN iram0
    0x5fff8000: instRam : iram0 : 0x8000 : executable, writable ;
     iram0_0 : C : 0x5fff8000 - 0x5fffffff : .iram0.text;
    END iram0
    
    BEGIN sram
    0x60000000: sysram : sram : 0x2F800 : executable, writable ;
     sram0 : F : 0x60000000 - 0x6000017b : .WindowVectors.text .Level2InterruptVector.literal;
     sram1 : F : 0x6000017c - 0x6000019b : .Level2InterruptVector.text .Level3InterruptVector.literal;
     sram2 : F : 0x6000019c - 0x600001bb : .Level3InterruptVector.text .DebugExceptionVector.literal;
     sram3 : F : 0x600001bc - 0x600001db : .DebugExceptionVector.text .KernelExceptionVector.literal;
     sram4 : F : 0x600001dc - 0x600001fb : .KernelExceptionVector.text .UserExceptionVector.literal;
     sram5 : F : 0x600001fc - 0x6000021b : .UserExceptionVector.text .DoubleExceptionVector.literal;
     sram6 : F : 0x6000021c - 0x6002f7ff :  STACK :  HEAP : .DoubleExceptionVector.text .sram.rodata .rodata .sram.literal .literal .sram.text .text .sram.data .data .sram.bss .bss;
    END sram
    
    

    You can use gdbio_sram as a reference for your flash LSP. Then in Xplorer, go to properties, and select your new LSP before building.

    You need to rebuild reset_vector.o every time you change the LSP, so I suggest you add the following command as a pre-build step:

    xt-clang --xtensa-core=hifi3z_lark_RI_2022_10 -mlsp= .\gdbio_flash -DXTOS_UNPACK -g -c -mlongcalls -mtext-section-literals -I "C:\usr\xtensa\XtDevTools\install\tools\RI-2022.10-win32\XtensaTools\xtensa-elf\src\xtos" -o  C:\usr\xtensa\XtDevTools\install\builds\RI-2022.10-win32\hifi3z_lark_RI_2022_10\xtensa-elf\arch\lib\reset-vector.o  C:\usr\xtensa\XtDevTools\install\tools\RI-2022.10-win32\XtensaTools\xtensa-elf\src\xtos\xea2\reset-vector-xea2.S

    When converting the elf file into hex, the addresses should be updated too:

    xt-dumpelf --base=0x68000000 --width=32 --full --size=0x30000 --little-endian .\bin\hifi3z_lark_swupgrade\Debug\dmic_dac_flashV2> dmic_dac_flashV2.hex

    By following these steps and using selfboot=high, room_boot=high, you should see your program being loaded and executed from flash just after reset. I hope this helps! Please let us know if you encounter additional problems.

    Kind regards,
    Roberto.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.