Post Go back to editing

AD1938 55 Hz noise

Category: Hardware
Product Number: AD1938

Hello again all!

I'm having a bit of trouble with my AD1938 setup. I have an board design that has a ADAU1462 in conjunction with AD1938 that feeds audio into PAs and then into speakers.

My problem is that the audio has a huge amount of noise in it. Upon inspection with an oscilloscope, It looks like a brief DC that is in the signal at a rate of 55Hz. This appears right at the output pin of the AD1938. I have tested out the power rails and everything to see if there's a similar signal elsewhere, but there is no indication that this is an external noise interference. It looks like the AD1938 is generating it.

I'm not sure if something in my code is incorrect, either in the DAC or the DSP (the DSP program is thus far a pass-through for S/PDIF plus 2 sinusoid sources for testing. I have some screenshots below. I just don't see these values corresponding to any kind of frequency from either of the chips, and it doesn't seem to be from the power rails. The power supply is an SMPS, further regulated by an LDO down to 3.3V and a Linear regulator for 5V.

The waveform you see the output from the Analog Devices' recommended op-amp interpolation filters. I copied the design exactly as specified in the AD1938 datasheet - I do not think these op-amps are to blame for this noise. And yes, I did test the output pin of the AD1938s to verify the noise starts there.

I'm hoping some of you AD1938 veterans might be able to sniff out what's wrong here. I do know that my SMPS is a cheap acquisition for quick and dirty testing, and I wouldn't be surprised if it were the source of the noise, however as I mentioned, I checked the SMPS power rails (which directly feed power to the PAs on the board), as well as the two regulator outputs. None of these sources show noise anywhere near this low frequency (as you'd expect, they do have a few mV here and there in the upper kHz region). I tried to put big bulk capacitors on the SMPS output terminals to try and snub anything that might be coming out - there was no appreciable difference in noise level from the speakers. I'm inclined to dismiss the power supplies as culprits.

Thank you in advance!