Post Go back to editing

Does the Input and output filter required for the codec

Category: Hardware
Product Number: AD1938

Hi Support  Team,

We are currently designing a new audio board utilizing the AD1938 codec, and we plan to use only one channel for input (ADC1LP, ADC1LN) and output (OL1, OR1). Given our application's low-end requirements, we do not necessitate high audio precision or quality.

After reviewing the user guides UG-045 and UG-87, we noticed that both schematics incorporate input and output filters. We understand that these filters serve two primary purposes: 1) converting single-ended inputs to differential-ended signals, and 2) shifting the signal reference from ground to 1.5V.

We would appreciate guidance on the following queries:

  1. Is it possible to eliminate the use of input and output filters, considering our goal to minimize the bill of materials (BOM) cost and reduce the board's size?

  2. If filters are unavoidable, can we utilize +12V/0V for the op-amp(ADA4075-2ARZ-R7) supply, given that +12V and +3.3V (for the codec) will be readily available?

We appreciate your support and look forward to your input on this matter.

Best regards,
Avnendra