Hi Support Team,
We are currently designing a new audio board utilizing the AD1938 codec, and we plan to use only one channel for input (ADC1LP, ADC1LN) and output (OL1, OR1). Given our application's low-end requirements, we do not necessitate high audio precision or quality.
After reviewing the user guides UG-045 and UG-87, we noticed that both schematics incorporate input and output filters. We understand that these filters serve two primary purposes: 1) converting single-ended inputs to differential-ended signals, and 2) shifting the signal reference from ground to 1.5V.
We would appreciate guidance on the following queries:
-
Is it possible to eliminate the use of input and output filters, considering our goal to minimize the bill of materials (BOM) cost and reduce the board's size?
-
If filters are unavoidable, can we utilize +12V/0V for the op-amp(ADA4075-2ARZ-R7) supply, given that +12V and +3.3V (for the codec) will be readily available?
We appreciate your support and look forward to your input on this matter.
Best regards,
Avnendra