Hello,
i'm wondering if i can connect two i2s component handling each 8 channels to only one audio serial interface on the ADAU1787 ?
one component is master, the other one is slave.
Each are configured in TDM mode [8 channels, 16 bits (16 BLCK per frame)]
i know the ADAU1787 has two ASI but i wanted to keep ASI2 available for another interface.
Initially, i selected ADAU1467 which supports 4 ASI but the TDM mode (seems to) do not support only 16 BCLK per frame (only 32 bits/channels)
This parameter seems to be configurable in the ADAU1787 (Serial Port x Control 1 register)
Thank you