Post Go back to editing

MAX98090 differential output to line input

Category: Hardware
Product Number: MAX98090

Hello,

I would like to use MAX98090 IC for and audio project.
Requirements:
stereo differential (configurable to single ended would be great) line level input
mono microphone input with noise gate and automatic level control
stereo differential line level output
I2S port


MAX98090 seems to be almost perfect for my project, but unfortunately it has D class differential amplifiers. I do not have experience with audio filters.
My question: do you have any experience regarding connecting output of this IC to another stage's line level input? Any application note?

I could use ADAU1361, that has line level stereo output, but I can't use the automatic level control feature, because I shall connect the mic to the aux input. I checked SSM2167 and MAX9814 as a preamp with ALC that could be connected to the ADAU aux input, but the overall cost would be much higher this way and ALC parameters could not be changed based on the connected mic with software.

I checked all AD codecs, and could not find a better one.