MAX9860
Production
The MAX9860 is a low-power, voiceband, mono audio codec designed to provide a complete audio solution for wireless voice headsets and other mono voice...
Datasheet
MAX9860 on Analog.com
MAX98089
Production
The MAX98089 is a full-featured audio codec whose high
performance and low power consumption make it ideal for
portable applications.
Class D speaker amplifiers...
Datasheet
MAX98089 on Analog.com
MAX98090
Production
The MAX98090 is a fully integrated audio codec whose high-performance, ultra-low power consumption and small footprint make it ideal for portable applications...
Datasheet
MAX98090 on Analog.com
Hello, Kaushalya,
1. The MAX9860 is intended to drive a mono headphone speaker. It is able to drive an 8Ω speaker, but the volume would be much lower than what can be provided by a speaker amplifier. The output will also likely become more distorted at lower power than with a 16Ω - 32Ω speaker.
If you look at the "HEADPHONE OUTPUT POWER vs. LOAD RESISTANCE" plot on page 9 of the datasheet, you can see that the "sweet spot" for output power is tuned for a 16Ω load. The output power line is illustrating the maximum power at a specific THD+N level, and the performance decreases quickly as the impedance goes below 16Ω.
2. There is no output over power limit function, because the MAX9860 cannot provide enough power to cause damage.
3. Yes, this is the appropriate method for using a single-ended microphone.
I am more familiar with legacy Maxim products so I don't have complete Analog Devices lineup information, but perhaps a CODEC with dedicated 8Ω speaker outputs would be more suitable for your application, like the MAX98089 or the MAX98090.
Hello, Kaushalya,
1. The MAX9860 is intended to drive a mono headphone speaker. It is able to drive an 8Ω speaker, but the volume would be much lower than what can be provided by a speaker amplifier. The output will also likely become more distorted at lower power than with a 16Ω - 32Ω speaker.
If you look at the "HEADPHONE OUTPUT POWER vs. LOAD RESISTANCE" plot on page 9 of the datasheet, you can see that the "sweet spot" for output power is tuned for a 16Ω load. The output power line is illustrating the maximum power at a specific THD+N level, and the performance decreases quickly as the impedance goes below 16Ω.
2. There is no output over power limit function, because the MAX9860 cannot provide enough power to cause damage.
3. Yes, this is the appropriate method for using a single-ended microphone.
I am more familiar with legacy Maxim products so I don't have complete Analog Devices lineup information, but perhaps a CODEC with dedicated 8Ω speaker outputs would be more suitable for your application, like the MAX98089 or the MAX98090.
Thanks Ed,
I can see your point regarding the 8 Ohms speaker. I have missed the Output power Vs load resistance graph. Thanks for pointing it out.
Cheers,
Kay