Post Go back to editing

Digital noise cancelling stethoscope

Thread Summary

The user is designing a digital stethoscope with noise cancellation using two Digital MEMs microphones. The ADAU1860 is recommended for its low latency fast DSP and HiFi core, suitable for noise cancellation and processing. Alternatives include the ADAU1787 and ADAU1788, which have a SigmaDSP core and are suitable for mono applications. The ADAU1797 is also an option with a more capable fast DSP and a Class-D headphone amplifier. The user should verify if a license is needed for the HiFi core in the ADAU1797.
AI Generated Content
Category: Hardware
Product Number: ADAU1850

We are designing a digital stethoscope with noise cancelling having two Digital MEMs microphones - one for listening to the Heart and lung sounds and one for the environment for noise cancellation. We need Audio codec with programmable DSP and headphone amplifier for the purpose. the ADAU1850 seems to be an overkill. Please suggest the appropriate part which fits the requirement. Shall we be needing a preamplifier like MAX9813H too in this case?