I would like to save a sound file inside the sigma or fast DSP so that I can use it to process with some white noise and get an output.
Is it possible to add a sound file in the system?
if yes. How?
ADAU1787
Recommended for New Designs
The ADAU1787 is a codec with four inputs and two outputs that incorporates two digital signal processors (DSPs). The path from the analog input to the...
Datasheet
ADAU1787 on Analog.com
I would like to save a sound file inside the sigma or fast DSP so that I can use it to process with some white noise and get an output.
Is it possible to add a sound file in the system?
if yes. How?
SAIPRATHEEP - Moved from SigmaDSP Processors & SigmaStudio Dev. Tool to Speech Processing Solutions. Post date updated from Thursday, January 4, 2024 7:05 AM UTC to Thursday, January 4, 2024 7:05 AM UTC to reflect the move.
Hope ADI has returned from the holidays.
May i know how to store an audio file or a sound file or wav format into the ADAU1787?
Hi SAIPRATHEEP ,
The ADAU1787 is not capable of storing any format of audio file. The Sigma DSP and Fast DSP are for processing of the signal chain created in the associated Sigma Studio schematics.
I believe I also provided an answer to your question in this thread: How to store audio file into ADAU1787 - Q&A - SigmaDSP Processors & SigmaStudio Dev. Tool - EngineerZone (analog.com)
I think an alternative solution would be to connect audio from your PC or phone audio connected to the analog input (AIN) of the ADC via 3.5mm aux cable, and then utilize the adder and white noise source block to combine these signals, which could then be routed to the stereo output.
I think the project file in the other thread I linked would serve as a great starting point to achieve your desired setup.
Please let me know if have any issues using the project file to get your desired setup or have any further questions. Thanks!
Best,
TBM