ADAU1467
Recommended for New Designs
The ADAU1463/ADAU1467 are automotive qualified audio processors that far exceed the digital signal processing capabilities of earlier SigmaDSP® devices...
Datasheet
ADAU1467 on Analog.com
SigmaStudio repeatedly throws up an error saying incompatible sampling rates detected. How do I fix this?
This error occurs when a module in SigmaStudio gets an input at a different sampling rate than what it expects. Please hover over the connections and check what the sampling rate is on that connection.
You can use the option on the top to set the sampling rate of new modules or change the sampling rate of all the modules in the schematic.
This error occurs when a module in SigmaStudio gets an input at a different sampling rate than what it expects. Please hover over the connections and check what the sampling rate is on that connection.
You can use the option on the top to set the sampling rate of new modules or change the sampling rate of all the modules in the schematic.