Post Go back to editing

I2S slave mode

Thread Summary

The user encountered an issue with no sound output when converting an 8-channel TDM signal to a 2-channel stereo I2S signal using the ADAU1452 in I2S slave mode. The problem was resolved by ensuring the TDM DATA signal was properly output, allowing the DSP to receive a valid data signal. The engineer also suggested using ASRC on the output side due to different clock domains and verifying the amplifier's I2S configuration.
AI Generated Content
Category: Software
Product Number: ADAU1452

Hello ADI team/community,

I need some help with the following issue.

My previous project used TDM signal input and converted it to I2S master mode(output); the outputs from OUT0–OUT3 were normal.

Now I need to change the project output to (I2S slave mode). In testing, OUT0 has data output, but there is no sound when it is connected to the power amplifier. Please help me check where the configuration in the project is wrong.

Thank you.ADAU1452-ba062.dspproj

Edit Notes

output
[编辑人: jenkey2008 编辑时间: 27 Oct 2026 8:42 AM (GMT -4)]
Parents
  • Hello jenkey2008,

    1. The clocks for the serial input port and the serial output port come from different external clock domains. Additionally, a 12.288MHz active crystal oscillator is used as the MCLK for the DSP.

    >> So, you have to use ASRC in the output side as well, since the core sample rate and serial output sample rate domain is different. Anyway, this is a recommended way for not getting any clicks and pops, but it won't be reason for no audio output.

    This is how to use ASRC in output side. This example shows routing DSP output to ASRC and then to serial output port 0.

    2.The serial output port has clock input, and also has data output.

    >> It seems the DSP outputs data correctly at the serial output port, so Has the amplifier configured correctly for input I2S?

    The level meter shows the signal is inside DSP, the serial port outputs data, which means it gets valid clocks. So, it has to be something in the AMP receiver side. A screenshot of the I2S signal would be helpful. 

    3.I would like to describe the engineering requirement I want to achieve: using the ADAU1452 to convert the input 8-channel TDM signal (serial input port 2) into a 2-channel stereo I2S signal (serial output port 0) for the downstream amplifier chip.

    >> It's a very possible configuration, so it can be surely done. And it seems your TDM8 signal is inside DSP and serial output port 0 outputs I2S signal, so it must be something in the AMP receiving side or any format corruption. if you can attach the scope images, it will be helpful.

    Regards,

    Harish

  • Hello Harish,

    Thank you for your kind help. I think my problem has been solved. The issue was that I overlooked the fact that the TDM DATA signal was not being output, so the DSP did not receive a valid data signal.

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.