We are using the MAX9737ETG+ class D amplifier in a non standard way (integrator and summing feedback paths) connected to a voltage transformer. This detail may be relevant or not.

The input signal is a 50Hz sine wave. When the input sine wave is too large then the OUT+ and OUT- signals distort but the differential output voltage is still a good sine wave. Is this normal?
I also expected the average voltage on OUT+ and OUT- of the class D amplifier to be PVDD / 2 = +12V / 2 = 6V but the average voltage is actually 1.69V. Is this normal?
Does this mean that the output signal is supposed to swing around COM (2.06V)?

Thanks in advance,
Pieter