Hello, I have a question. According to the specification sheet, MAX4466 and MAX4468 are both in the same specification sheet. However, from the schematic diagram, MAX4466 takes the input signal from the IN+ pin, while MAX4468 takes the input signal from the IN- pin. Does this indicate that they are not the same type of amplifier?